Skip to main content
Nikolai_Werenich
Visitor II
December 9, 2021
Question

stm32f373r8t6 - CAN not working at 1Mbit / s

  • December 9, 2021
  • 1 reply
  • 998 views

Hello forum users!

Created a project by example

[url] https://istarik.ru/blog/stm32/159.html [/ url]

Slightly corrected, so that a new frame is sent every 10 msec.

The project works at (except one) any speed (100kbit - works, 500, 800 - works).

Data is transmitted and received by a usb-can converter (sys tec elecronic).

Here, for example, I configured the project for a CAN speed of 500kbit / s:

- here is the CAN tincture:

[url = http: //vfl.ru/fotos/6049ccb837010333.html] [img] http://images.vfl.ru/ii/1638964027/6049ccb8/37010333_m.jpg [/ img] [/ url]

- and here is the frequency setting:

[url = http: //vfl.ru/fotos/d34be44637010398.html] [img] http://images.vfl.ru/ii/1638964156/d34be446/37010398_m.jpg [/ img] [/ url]

-and this data is received at a speed of 500 kbps:

[url = http: //vfl.ru/fotos/2ec1947737010697.html] [img] http://images.vfl.ru/ii/1638965166/2ec19477/37010697_m.jpg [/ img] [/ url]

- this is the picture on the CAN bus:

[url = http: //vfl.ru/fotos/d52d156337010759.html] [img] http://images.vfl.ru/ii/1638965437/d52d1563/37010759_m.jpg [/ img] [/ url]

************************************************* *********

Okay, reconfiguring the speed to 1Mbps.

To do this, you just need to change the CAN frequency divider from 4 to 2.

And Cube kindly calculates the bus speed:

[url = http: //vfl.ru/fotos/75dbe36237010531.html] [img] http://images.vfl.ru/ii/1638964501/75dbe362/37010531_m.jpg [/ img] [/ url]

I'm flashing the microcontroller and that's it. Data is not accepted :(, but on the bus this is the picture:

- to fit everything into the monitor, I had to change the sweep to 100msec !!!!

[url = http: //vfl.ru/fotos/b265ca8237010856.html] [img] http://images.vfl.ru/ii/1638965896/b265ca82/37010856_m.jpg [/ img] [/ url]

At the same time, if you look at the status of the registers, then CAN reports and sets error bits:

[url = http: //vfl.ru/fotos/75f6ccfa37010945.html] [img] http://images.vfl.ru/ii/1638966181/75f6ccfa/37010945_m.jpg [/ img] [/ url]

LEC Bits in ESR Register: 101: Bit dominant Error

Why does stm32 not want to work at a CAN speed of 1 Mbit / s ???

This topic has been closed for replies.

1 reply

mƎALLEm
ST Technical Moderator
December 9, 2021

Hello @Nikolai_Werenich​ ,

Could you please increase the system clock to 72MHz (AHB prescaler = 1, APB1 prescaler = 2)?

Also for the sample point it's recommended to set it at about 88% of the bit time at higher bitrates.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.