Question
STM32F373 SDADC (Sigma-Delta ADC)
Posted on March 18, 2014 at 03:12
Hello,
I am planning on using the SDADC in STM32F37x microcontroller. The data sheets says the sampling frequency is between 500 kHz ~ 6 MHz, depending on the clock signal driving the SDADC. The output data rate is 4.167 ksps ~ 50 ksps accordingly. So it appears that the over sampling rate is 120. But the data sheet never says so. In between these two points, I can drive the SDADC with a clock signal derived from the system clock and get a output data rate of 1/120 of the frequency of the driving clock signal. Am I correct? Thanks for your input. Jim #stm32f373-sdadc