Skip to main content
Jean Paul Talledo Vilela
Associate II
Mar 6, 2018 8:04 PM UTC
Question

STM32F373 Jlink/JTAG issue after setting Clock

Posted on March 06, 2018 at 21:04

Hi

I am trying to debug my program and every time I go to the SystemClock_Config() function my Jlink debugger shows errors and doesn't work anymore.

I am using an external crystal ( 8Mhz) but I changed my clock to internal thinking that was the problem.

Here is my function contents:

void SystemClock_Config(void)

{

  RCC_OscInitTypeDef RCC_OscInitStruct;

  RCC_ClkInitTypeDef RCC_ClkInitStruct;

  RCC_PeriphCLKInitTypeDef PeriphClkInit;

    /**Initializes the CPU, AHB and APB busses clocks

    */

  /*

  RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_LSI|RCC_OSCILLATORTYPE_HSE;

  RCC_OscInitStruct.HSEState = RCC_HSE_ON;

  RCC_OscInitStruct.HSEPredivValue = RCC_HSE_PREDIV_DIV1;

  RCC_OscInitStruct.HSIState = RCC_HSI_ON;

  RCC_OscInitStruct.LSIState = RCC_LSI_ON;

  RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;

  RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;

  RCC_OscInitStruct.PLL.PLLMUL = RCC_PLL_MUL9;

  if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)

  {

    _Error_Handler(__FILE__, __LINE__);

  }*/

  /**Configure LSE Drive Capability

    */

  __HAL_RCC_LSEDRIVE_CONFIG(RCC_LSEDRIVE_LOW);

    /**Initializes the CPU, AHB and APB busses clocks

    */

  RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORTYPE_LSE;

  RCC_OscInitStruct.LSEState = RCC_LSE_ON;

  RCC_OscInitStruct.HSIState = RCC_HSI_ON;

  RCC_OscInitStruct.HSICalibrationValue = 16;

  RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;

  RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;

  RCC_OscInitStruct.PLL.PLLMUL = RCC_PLL_MUL16;

  if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)

  {

    _Error_Handler(__FILE__, __LINE__);

  }

    /**Initializes the CPU, AHB and APB busses clocks

    */

  RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK

                              |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;

  RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;

  RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;

  RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;

  RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;

  if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)

  {

    _Error_Handler(__FILE__, __LINE__);

  }

  PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_USART1|RCC_PERIPHCLK_USART3

                              |RCC_PERIPHCLK_RTC|RCC_PERIPHCLK_SDADC;

  PeriphClkInit.Usart1ClockSelection = RCC_USART1CLKSOURCE_PCLK2;

  PeriphClkInit.Usart3ClockSelection = RCC_USART3CLKSOURCE_PCLK1;

  PeriphClkInit.RTCClockSelection = RCC_RTCCLKSOURCE_LSI;

  PeriphClkInit.SdadcClockSelection = RCC_SDADCSYSCLK_DIV12;

  if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)

  {

    _Error_Handler(__FILE__, __LINE__);

  }

  HAL_PWREx_EnableSDADC(PWR_SDADC_ANALOG1);

  HAL_PWREx_EnableSDADC(PWR_SDADC_ANALOG3);

    /**Configure the Systick interrupt time

    */

  HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);

    /**Configure the Systick

    */

  HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);

  /* SysTick_IRQn interrupt configuration */

  HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);

}

So, when I enter in debug mode, pretty much the debugger stops working when I called this function:

        /* Enable the main PLL. */

        __HAL_RCC_PLL_ENABLE();

which it is inside stm32f3xx_hal_rcc.c and function:

HAL_StatusTypeDef HAL_RCC_OscConfig(RCC_OscInitTypeDef  *RCC_OscInitStruct)

Any suggestions?

My setup is using a custom board with STM32F373CCTx, JLink in JTAG Mode

Thanks in advance!!

    This topic has been closed for replies.

    1 reply

    Jean Paul Talledo Vilela
    Associate II
    Mar 7, 2018 1:50 PM UTC
    Posted on March 07, 2018 at 14:50

    Doing more debugging, looks like the issue happens when I select to use the PLL. Either HSI or HSE wont work. Currently I am stuck running at 8 MHZ with the internal clock.

    I verified the Flash Preempt is enabled and 2 Wait States had been added to the FLASH->ACR.