Question
stm32f373 adc ftrig
Posted on October 30, 2017 at 05:13
Hi,
Looking at the other stm32 MCU's like the stm32f407 I see in their datasheet a spec fTRIG (aka the External trigger frequency) ... however I cannot see the same spec for the 16bit SDADC on the stm32f373 datasheet ... indeed it is even there for the stm32f373 12 bit ADC.
It seems I can trigger an ADC via the JEXTSEL bits from an EXTI11 line or a TIM TRGO output etc just like for all the other ADC's. What is the max trigger frequency for this please (or did I miss it)?
Thanks
#stm32f373-adc-trigger #stm32f373 #synchronize