Question
STM32F373
Posted on November 05, 2015 at 11:33
Dear Community,
I want to use all the 3 DACs of a stm32f373 device. All of them need to be feed by DMA and triggered by the same external trigger impulse. Unfortunately none of the DACs is outputting anything. I use the following initialization code. I would be very if someone could review the code and if possible point me into the right direction
void DAC123_Init() {
/* Preconfiguration before using DAC----------------------------------------*/
//DAC_Config
GPIO_InitTypeDef GPIO_InitStructure;
DAC_InitTypeDef DAC_InitStructure;
DMA_InitTypeDef DMA_InitStructure;
NVIC_InitTypeDef NVIC_InitStructure; //DMA Interupt
//Enable GPIOA (PA4,5 & 6) as DAC output
// GPIOA clock enable
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);
// Configure PA.04 (DAC_OUT1) as analog
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_Init(GPIOA, &GPIO_InitStructure);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_5;
GPIO_Init(GPIOA, &GPIO_InitStructure);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6;
GPIO_Init(GPIOA, &GPIO_InitStructure);
//*************************************************************************
// DMA1 clock enable (to be used with DAC)
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_DMA1, ENABLE);
// DAC Periph clock enable RCC_APB1Periph_DAC1
RCC_APB1PeriphClockCmd(RCC_APB1Periph_DAC1, ENABLE);
RCC_APB1PeriphClockCmd(RCC_APB1Periph_DAC2, ENABLE);
DAC_DeInit(DAC1);
DAC_DeInit(DAC2);
// DAC1 channel1 and channel2
// DAC2 channel
DAC_InitStructure.DAC_Trigger = DAC_Trigger_Ext_IT9;
DAC_InitStructure.DAC_WaveGeneration = DAC_WaveGeneration_None;
DAC_InitStructure.DAC_OutputBuffer = DAC_OutputBuffer_Enable;
DMA_DeInit(DMA1_Channel3);
DMA_DeInit(DMA1_Channel4);
DMA_DeInit(DMA1_Channel5);
DMA_InitStructure.DMA_MemoryBaseAddr =
(uint32_t)&(DAC_BufferX);
DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;
DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord
DMA_InitStructure.DMA_PeripheralBaseAddr =
(uint32_t)&DAC1->DHR12R1;
DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralDST;
DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;
DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord;
DMA_InitStructure.DMA_BufferSize = 201;
DMA_InitStructure.DMA_Mode = DMA_Mode_Circular;
DMA_InitStructure.DMA_Priority = DMA_Priority_High;
DMA_InitStructure.DMA_M2M = DMA_M2M_Disable;
DMA_Init(DMA1_Channel3, &DMA_InitStructure);
DMA_InitStructure.DMA_MemoryBaseAddr = (uint32_t)&(DAC_BufferY);
DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)&DAC1->DHR12R2;
DMA_Init(DMA1_Channel4, &DMA_InitStructure);
DMA_InitStructure.DMA_MemoryBaseAddr = (uint32_t)&(DAC_BufferZ);
DMA_InitStructure.DMA_PeripheralBaseAddr =
(uint32_t)&DAC2->DHR12R1;
DMA_Init(DMA1_Channel5, &DMA_InitStructure);
//Interupts
//DMA_IT_TC: Transfer complete interrupt mask
//DMA_IT_HT: Half transfer interrupt mask
//DMA_IT_TE: Transfer error interrupt mask
// Enable DMA1 channel3 IRQ Channel
// Enable DMA1 channel4 IRQ Channel
// Enable DMA1 channel5 IRQ Channel
NVIC_InitStructure.NVIC_IRQChannel = DMA1_Channel3_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
NVIC_InitStructure.NVIC_IRQChannel = DMA1_Channel4_IRQn;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1;
NVIC_Init(&NVIC_InitStructure);
NVIC_InitStructure.NVIC_IRQChannel = DMA1_Channel5_IRQn;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 2;
NVIC_Init(&NVIC_InitStructure);
// DMA CONFIG
DMA_ITConfig(DMA1_Channel3, DMA_IT_TC | DMA_IT_HT, ENABLE);
DMA_Cmd(DMA1_Channel3, ENABLE);
DMA_ITConfig(DMA1_Channel4, DMA_IT_TC | DMA_IT_HT, ENABLE);
DMA_Cmd(DMA1_Channel3, ENABLE);
DMA_ITConfig(DMA1_Channel5, DMA_IT_TC | DMA_IT_HT, ENABLE);
DMA_Cmd(DMA1_Channel3, ENABLE);
//DAC INIT
DAC_Init(DAC1, DAC_Channel_1, &DAC_InitStructure);
DAC_Init(DAC1, DAC_Channel_2, &DAC_InitStructure);
DAC_Init(DAC2, DAC_Channel_1, &DAC_InitStructure);
//DAC ENABLE
DAC_Cmd(DAC1,DAC_Channel_1, ENABLE);
DAC_Cmd(DAC1,DAC_Channel_2, ENABLE);
DAC_Cmd(DAC2,DAC_Channel_1, ENABLE);
// Enable DMA for DAC Channels
DAC_DMACmd(DAC1, DAC_Channel_1, ENABLE);
DAC_DMACmd(DAC1, DAC_Channel_2, ENABLE);
DAC_DMACmd(DAC2, DAC_Channel_1, ENABLE);
}