Skip to main content
Uwe Bonnes
Chief
November 6, 2017
Question

STM32F37 USB implemenatation

  • November 6, 2017
  • 3 replies
  • 656 views
Posted on November 06, 2017 at 15:12

Hello,

STM32F37 reference manual rm0313.pdf Rev5 in chaper 29.3 'USB implementation' lists 2 implementations, one with 512 byte and the second with 1024 byte packet memory. There is no explanation when which implementation applies.

The system header only list  USB for STM32F373, while STM32F378 has no USB.

What holds/

    This topic has been closed for replies.

    3 replies

    Uwe Bonnes
    Chief
    November 6, 2017
    Posted on November 06, 2017 at 15:37

    In Table 106 'USB implementation' I also doubt about the '2x 16 bits/word' Dedicated packet buffer memory SRAM access scheme. Looking with the debugger all halfwords on odd halfword addresses are zero and not writable. This probably also has consequences to Table 1 'Table 1. STM32F37xxx peripheral register boundary addresses (continued)' for the USB related entry. Probably 0x40006000 up to 0x400063fff is used for USB packet memory. In table 1 entry '0x4000 6200 - 0x4000 63FF ' has also the wrong size '1 KB'

    Amel NASRI
    ST Technical Moderator
    November 6, 2017
    Posted on November 06, 2017 at 16:42

    Hi

    Bonnes.Uwe

    ‌,

    There is an error in the table 106 ''USB implementation'' of the RM0313: the 3rd column will be removed as it shouldn't be there.

    Then, the last line ''USB 2.0 Link Power Management (LPM) support'' has to be removed as LPM isn't supported in STM32F Accordingly, all LPM related bits have to marked as reserved in USB registers.

    This is already tracked to be fixed in coming RM version.

    Regarding table 1, we have the following:

    0690X00000608rbQAA.png

    The entry

    entry ''0x4000 6200 - 0x4000 63FF'' is reserved, that is true it should be 0.5 KB.

    -Amel

    To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
    Uwe Bonnes
    Chief
    November 6, 2017
    Posted on November 06, 2017 at 17:16

    What about the '2x 16 bits/word' issue? I am sure the Stm32f3& USB has '1x16/vord'! As explained above, this has consequences to Table 1