STM32F334R8T6 can not read memory
- April 12, 2018
- 0 replies
- 759 views
I have designed a board with STM32F334R8T6. The STM32 pins are configured as in the attached file (I do not think there is a problem here since I have already used the same configuration without problems). The microcontroller is programmed with a STM32 NUCLEO BOARD using the 6-pins connector (3.3V, PA14, GND, PA13, NRST, PB3): also in this case I do not think there is a problem since I can program without problems other boards using the same NUCLEO board and connector.
When I try to connect to the STM32F334 microcontroller using STM32 ST-LINK utility I get the following message:
09:33:
03
: ST-LINK SN : 066BFF515056805087143648
09:33:
03
: ST-LINK Firmware version : V2J21M5
09:33:
03
: Connected via SWD.
09:33:
03
: Connection mode : Connect Under Reset.
09:33:
03
: Debug in Low Power mode enabled.
09:33:
04
: Device ID:0x438
09:33:
04
: Device flash Size : 64KBytes
09:33:
04
: Device family :STM32F303x4-x6-x8/F328xx/F334xx
09:33:
05
: Failed to read memory @08010000!
The programmer seems not to be able to access the microcontroller flash memory. However I can not figure out the reason for this.
If I try to program the microcontroller the following messages are displayed
10:01:45 : [Prova_F334.bin] opened successfully.
10:01:47 : Memory-Loader error10:01:47 : Error occured during erase operation!The option bytes are set according to the attached file.
Can anyone help to solve this problem?
Thanks.
#memory-map #stm32f334 #program-memory #flash-corrupt #memory-configuration