Skip to main content
Jordi Becares
Associate III
Nov 21, 2018 10:00 AM UTC
Question

STM32F334, Use HAL lib to configure ADC with EXTI 11 as trigger + DMA

Hi,

I'm trying to configure ADC2 to get data via DMA with external trigger interrupt.

I'm usign StCube framework.

I get read data via DMA with request capture via software with any problem, but I need to synchronise the external trigger with start ADC via HW (If i capture the external interrupt and after enable ADC, I have a big delay of 4us)

HAL_ADC_Start_DMA(&hadc2, (uint32_t*)buffDMA, 100)

But, I don't know how to start DMA when config EXTI

Here, code to config ADC with EXTI line 11

/* ADC2 init function */
static void MX_ADC2_Init(void)
{
 
 ADC_ChannelConfTypeDef sConfig;
 
 /**Common config 
 */
 hadc2.Instance = ADC2;
 hadc2.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1;
 hadc2.Init.Resolution = ADC_RESOLUTION_8B;
 hadc2.Init.ScanConvMode = ADC_SCAN_DISABLE;
 hadc2.Init.ContinuousConvMode = ENABLE;
 hadc2.Init.DiscontinuousConvMode = DISABLE;
 hadc2.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_RISING;
 hadc2.Init.ExternalTrigConv = ADC_EXTERNALTRIGCONV_EXT_IT11;
 hadc2.Init.DataAlign = ADC_DATAALIGN_RIGHT;
 hadc2.Init.NbrOfConversion = 1;
 hadc2.Init.DMAContinuousRequests = DISABLE;
 hadc2.Init.EOCSelection = ADC_EOC_SEQ_CONV;
 hadc2.Init.LowPowerAutoWait = DISABLE;
 hadc2.Init.Overrun = ADC_OVR_DATA_OVERWRITTEN;
 if (HAL_ADC_Init(&hadc2) != HAL_OK)
 {
 _Error_Handler(__FILE__, __LINE__);
 }
 
 
 /**Configure Regular Channel 
 */
 sConfig.Channel = ADC_CHANNEL_1;
 sConfig.Rank = ADC_REGULAR_RANK_1;
 sConfig.SingleDiff = ADC_SINGLE_ENDED;
 sConfig.SamplingTime = ADC_SAMPLETIME_1CYCLE_5;
 sConfig.OffsetNumber = ADC_OFFSET_NONE;
 sConfig.Offset = 0;
 if (HAL_ADC_ConfigChannel(&hadc2, &sConfig) != HAL_OK)
 {
 _Error_Handler(__FILE__, __LINE__);
 }

Now, how start device to get data via DMA when interrupt in EXTI_11 is fired?

Thanks

Jordi

This topic has been closed for replies.