STM32F334 RTC Smooth Calibration
Hi,
Trying to calibrate the RTC, Using a LSE with 32768kHz xtal, which is running at a frequency of 32985.6Hz.
// with 32768Hz LSE, with AsynchPre=0x7f(128),
// CALIBOUT = 257.7Hz (measured on a scope)// 32768/128 = 256Hz, but output is 257.7Hz// 257.7Hz * 128 = 32985.6Hz// error in this situation: +217.6 pulses// 257.7 / 256.0 = 1.006640625Doing smooth calibration with the CALM bits appeared to the straightforward choice to do the error correction.
So, I did
// RTC Block diagram Fig:320 on Page #825 of the Reference Manual
// RTC_OUT can either Output RTC_CALIB or RTC_ALARM // RTC_CALIB is either 1Hz or 512Hz, which is derived from RTCCLK // RTC_OUT, RTC_TS, RTC_TAMP1 are mapped to the same pin PC.13// RTC Calib Output on PC.13
__GPIOC_CLK_ENABLE(); /* PC.13 CALIB_OUT */..
..
RTC_CalibOutputConfig(RTC_CalibOutput_1Hz);
RTC_CalibOutputCmd(ENABLE); /* 1Hz on PC.13 */ RTC_SmoothCalibConfig(RTC_SmoothCalibPeriod_8sec, RTC_SmoothCalibPlusPulses_Reset, RTC_CALR_CALM_7); /* subtract 127 clocks */I get the very same frequency on PC.13, irrespective of the CALM bits.
Am I on the right path ?
Wondering whether the PC.13 pin is supposed to reflect the changes set by Smooth Calibration ?
Can someone clarify ?
Thanks!