Skip to main content
KPrei
Visitor II
Jul 26, 2018 7:21 PM UTC
Question

STM32F303ZE software triggering of timers through the TIMx_EGR register

We are running TIM3 and TIM2 on a STM32F303ZE processor generating pulses on both timer outputs synchronous to an external input trigger. We have TIM3 configured for “Trigger Mode�? with the “External Trigger�? selected running in “one pulse mode�?. TIM2 is slaved to TIM3-TRGO which is selected as TIM3 Count Enable. The output pulses are generated on TIM3-CH2 (Retriggerable OPM mode 2) and TIM2-CH1 (PWM Mode 2).

The configuration works as expected when an external trigger is present. I would like to occasionally “trigger�? the pulses manually by writing the TG bit in the TIM3_EGR register but this does not work. It doesn’t even cause the TIM2 slave to trigger.  

I ran a couple experiments.  

1) By setting the counter enable bit in TIM3 CR1-CEN, TIM2 CH1 will generate it’s output pulse however, TIM3-CH2 does not generate an output pulse. 

2) I re-ran the first experiment but instead of running TIM3-CH2 in Retriggerable OPM mode 2 (9), I ran it in PWM mode 2 (7) and set CCR2 to 1. When I set the TIM3 counter enable bit, the TIM3-CH2 output changes meaning that simply starting the TIM3 counter does not enable the CH2 output channel when configured for Retriggerable OPM mode 2. Unfortunately, running in PWM mode 2 is no good since I need to set CCR2 to a non-zero value in order to generate a pulse and this delays the generated pulse.

Why does writing of the TG bit in the timer 3 event register not trigger output pulses on TIM3-CH2?  

Original TIM3 Configuration

CR1-UIREMAP = 0

CR1-CKD       = 0

CR1-ARPE      = 1

CR1-CMS       = 0

CR1-DIR        = 0

CR1-OPEM     = 1 (one pulse mode)

CR1-URS       = 0

CR1-UDIS       = 0

CR1-CEN       = 0

CR2-TI1S       = 0

CR2-MMS      = 1 (TRGO = CNT_EN)

CR2-CCDS      = 0

SMCR-ETP      = 0

SMCR-ECE      =0

SMCR-ETPS     = 0

SMCR-ETF      = 0

SMCR-MSM    = 1 (master mode enable)

SMCR-TS       = 7 (external trigger input ETRF)

SMCR-OCCS    = 0

SMCR-SMS     = 6 (Trigger Mode)

CCMR1-OC2M  = 9 (Retriggerable OPM mode 2)

CCMR1-OC2CE = 0

CCMR1-OC2PE = 0

CCMR1-OC2FE  = 0

CCMR1-CC2S   = 0

CCER-CC2NP   = 0

CCER-CC2P     = 0

CCER-CC2E     = 1 (enable CH2 output)

CNT            = 0

PSC            = 0x167

ARR            = 40000

CCR2           = 0 (no delay)

Thank you!

    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    Aug 10, 2018 3:30 AM UTC

    @ST Community​ any FAEs want to cover this?

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..