Skip to main content
Antonio Santoro
Visitor II
May 12, 2018 3:36 PM UTC
Question

STM32F303VC DAC signal generation and period measure using EXTI interrupt

Posted on May 12, 2018 at 17:36

I'm trying to generate a square wave signal using the DAC channel 2 (PA5) with a 1.627 ms period and then measuring that by catching the rising edge trigger in an EXTI4 interrupt on the PF4 pin. The problem is that I have to use the DAC channel 1 to see the EXTI4 triggers and the measured period is not what I expect to be.

This is the complete program, I'm working using IAR Embedded Workbench 8.22:

&sharpinclude 'header.h'

&sharpinclude <math.h>

&sharpinclude <stdio.h>

&sharpdefine N 100

//&sharpdefine tau 1.38*pow(10,-8)

int j=0, flag=0;

float periodi[N];

void setup(){

RCC->AHBENR |= RCC_AHBENR_GPIOAEN | RCC_AHBENR_GPIOFEN;

RCC->APB2ENR |= RCC_APB2ENR_SYSCFGEN;

RCC->APB1ENR |= RCC_APB1ENR_TIM2EN | RCC_APB1ENR_TIM3EN | RCC_APB1ENR_DACEN;

GPIOA->MODER |= GPIO_MODER_MODER5;

GPIOF->MODER |= GPIO_MODER_MODER4;

NVIC->ISER[0] |= (1<<10 | 1<<29);

SYSCFG->EXTICR[2] |= SYSCFG_EXTIRCR_EXTI4_PF;

EXTI->IMR |= EXTI_IMR_MR4;

EXTI->RTSR |= EXTI_RTSR_TR4;

}

void setupTIM2(){

TIM2->PSC = 71;

TIM2->CR1 |= TIM_CR1_CEN;

TIM2->CNT = 0;

}

// 65536 : 0.0009*PSC = 65536 : 0.8135 ==> PSC = 0.8135 / 0.0009 ==> PSC = 904

// 65536 : 0.8228 = ARR : 0.8135 ==> ARR = (65536 / 0.8228) * 0.8135 = 64795

void setupTIM3(){

TIM3->PSC = 903;

TIM3->ARR = 64795;

TIM3->DIER |= TIM_DIER_UIE;

TIM3->CR1 |= TIM_CR1_CEN;

TIM3->CNT = 0;

}

void TIM3_IRQHandler(){

TIM3->SR &= ~TIM_SR_UIF;

//printf('TIM3\n');

if(flag==0){

DAC->DHR12R1 = 0;

flag = 1;

for(int i=0; i<1000; i++);

}

else{

DAC->DHR12R1 = 4095;

flag = 0;

for(int i=0; i<1000; i++);

}

}

void EXTI4_IRQHandler(){

EXTI->PR |= EXTI_PR_PR4;

//printf('EXTI4\n');

if(j<N){

periodi[j] = TIM2->CNT*tau;

j++;

TIM2->CNT = 0;

}

else{

TIM2->CR1 &= ~TIM_CR1_CEN;

TIM3->CR1 &= ~TIM_CR1_CEN;

DAC->CR &= ~DAC_CR_EN1;

}

}

void setupDAC(){

DAC->CR |= DAC_CR_EN1;

}

void main(){

setup();

setupDAC();

setupTIM2();

setupTIM3();

while(1);

}

#exti-handler #interrupt #dac #stm32f3 #embedded-softwares
This topic has been closed for replies.