Skip to main content
EmbeddedErik
Associate II
April 12, 2023
Solved

STM32F303VB TIM15 PWM not working properly

Hello! I am working on PWM generation using several timers, in this case: TIM3, TIM4, TIM8, TIM15. I have gotten TIM3, TIM4 and TIM8 to work perfectly. I am currently testing this on a STM32F3DISCOVERY board. TIM15 however, does not behave properly for me. It uses the same code as for the other general purpose timers I use (Besides the code for CCR3 and CCR4 of course.

In this case, I use PF9 and PF10 with AF3 enabled. The registers show that AF3 is selected for these.

RCC Configuration:

RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM15, ENABLE);
 
RCC_AHBPeriphClockCmd((RCC_AHBPeriph_GPIOF), ENABLE);

GPIO configuration:

GPIO_InitTypeDef GPIO_InitStruct;
 
GPIO_PinAFConfig(GPIOF, GPIO_PinSource9, GPIO_AF_3);
GPIO_PinAFConfig(GPIOF, GPIO_PinSource10, GPIO_AF_3);
 
GPIO_StructInit(&GPIO_InitStruct);
GPIO_InitStruct.GPIO_Pin = GPIO_Pin_9 | GPIO_Pin_10;
GPIO_InitStruct.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStruct.GPIO_OType = GPIO_OType_PP;
GPIO_InitStruct.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_Init(GPIOF, &GPIO_InitStruct);

Code for the TimeBaseStructure config:

TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
 
 
/*Fill struct with default values*/
TIM_TimeBaseStructInit(&TIM_TimeBaseStructure);
 
/*Prescale AHB clock to give 64KHz*/
TIM_TimeBaseStructure.TIM_Prescaler = (1000 - 1);
 
/*Set the time ARR (auto-reload register value) to 64000*/
TIM_TimeBaseStructure.TIM_Period = (uint16_t)(64000 - 1);
 
/*No clock division and counting up to the ARR (auto-reload register) value*/
TIM_TimeBaseStructure.TIM_ClockDivision = 0;
TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
 
/*Initialize struct*/
TIM_TimeBaseInit(PWMTIMERx, &TIM_TimeBaseStructure);

OCInitStructure:

TIM_OCInitTypeDef TIM_OCInitStructure;
 
/*Fill struct with default values*/
TIM_OCStructInit(&TIM_OCInitStructure);
 
/*Setup for PWM modulated output signal*/
TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1;
TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
 
/*Set the pulse width (duty cycle) to 0 initially*/
TIM_OCInitStructure.TIM_Pulse = 0;
TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;
 
 
TIM_OC1Init(PWMTIMERx, &TIM_OCInitStructure);
TIM_OC1PreloadConfig(PWMTIMERx, TIM_OCPreload_Enable);
TIM_OC2Init(PWMTIMERx, &TIM_OCInitStructure);
TIM_OC2PreloadConfig(PWMTIMERx, TIM_OCPreload_Enable);

I did consider whether the PF9 and PF10 pins was connected to an internal function on the STMF3DISCOVERY, but I could perform a GPIO_SetBits without issues, and setting both to high/low, and the datasheet did not mention that it was used for anything. The issue is that i get no PWM output whatsoever on PF9 or PF10. I did my best to compare the registers between one of my working General purpose timers and TIM15, but they looked identical to me. Am I missing a small crucial step here?

Thank you in advance!

This topic has been closed for replies.
EmbeddedErik
EmbeddedErikBest answer
Associate II
April 12, 2023

Hi! For anyone else having this issue, I found out my issue:

The following line had to be added, I thought it was only for advanced timers.

TIM_CtrlPWMOutputs(TIM15, ENABLE);

2 replies

gbm
Super User
April 12, 2023

Check the TIMx->CCER register, which is modified by HAL_TIM_PWM_Start().

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice
EmbeddedErik
EmbeddedErikAuthorBest answer
Associate II
April 12, 2023

Hi! For anyone else having this issue, I found out my issue:

The following line had to be added, I thought it was only for advanced timers.

TIM_CtrlPWMOutputs(TIM15, ENABLE);