Skip to main content
AWeis
Visitor II
Jun 20, 2019 9:35 PM UTC
Question

STM32F303RE Nucleo Board HAL_USART_Receive_IT problem

As the title suggests, im having a problem using HAL to make some USART echo.

I tried the same approch on a nucleo-f031 and its working wonderfully.

I can print the whole hyperterminal string, but i cant reach the receive interrupt. Even if i set the RXNEIE bit manually it doesnt trigger the USART2 interrupt.

Just to clarify, i bridged both connection SB62 and SB63 so i can see the USART communication on a logic analyzer.

im hoping for help

This topic has been closed for replies.