Question
STM32F303RE 64-pin 4 SPIs?
Posted on September 19, 2016 at 19:07
Hi!
As i was searching for a STM32 with 4 SPI peripherals I stumbeld across the STM32F303RE. After consulting the manual, I am a bit confused: The webdescription and Feature list tells me, that there are 4 SPIs on all different 64-pin to 144-pin packages. But when I check the pinout description in the datasheet only 100 and 144-pin packages provide SPI1-4 capability. So what is wrong here? the datasheet or the overal description?Basically I want the small sized 4 SPI package. But is it now 64 or 100?best regardsBenjamin #spi #stm32f303re