Hi @EL_HACHIMI ,
A full-speed device uses a pull-up resistor attached to D+ to specify itself as a full-speed device (and to
indicate its speed). The pull-up resistor at the device end is also used by the host or hub to detect the presence of
a device connected to its port. Without a pull-up resistor, the USB assumes that there is nothing connected to the
bus.
On some STM32 microcontrollers, the pull-up resistor is already embedded. Otherwise, the customer needs to
add it. Refer to Embedded pull-up resistor on USB_DP line in table 3 in AN4879 to know if this resistor is integrated on the used STM32 MCU.
For STM32F303ZE, the USB_DP (D+) pin must be pulled up to a voltage in the 3.0 to 3.6 V range with a 1.5 kΩ resistor.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.