Skip to main content
Jiannong Zhou
Associate III
August 31, 2022
Question

STM32F303 UART 3 receiver hang without RX interrupt after run 1-2 hours.

  • August 31, 2022
  • 11 replies
  • 2350 views

I am using my boards with STM32F303VBT6, There is a UART 3 hang after run for 1-2 hours. There is no UART interrupt of the receiver. I monitored the RS232 signal is there.

After reset the receiver board, the receiving date can be recovered.

What is the possible reason to cause no UART 3 interrupt?

Best regards,

Jiannong

This topic has been closed for replies.

11 replies

Tesla DeLorean
Guru
August 31, 2022

>>What is the possible reason to cause no UART 3 interrupt?

Some error status' flagged which you fail to clear.

Show USART3->SR in these situations

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Jiannong Zhou
Associate III
August 31, 2022

Thanks Tesla for your suggestion. I will check it.

Tesla DeLorean
Guru
August 31, 2022

Things like framing, parity, noise, etc

Get flagged, and need clearing indivdually.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Jiannong Zhou
Associate III
September 1, 2022

Hi Tesla,

When the issue happened, HAL_UART_RxCpltCallback() does not call back again.

// UART call back

void HAL_UART_RxCpltCallback (UART_HandleTypeDef *huart)

{

if(huart->Instance == USART3)

{

....

}

}

How to check ISR, NE, ORE, FE and clear them?

Jiannong

Jiannong Zhou
Associate III
September 1, 2022

Hi Tesla,

  1. Normal work: ISR = 0x6210D0
  2. Issue happens: ISR = 0x6210F8

Jiannong

Jiannong Zhou
Associate III
September 1, 2022

Hi Tesla,

The difference is D3 and D5 set.

USART_ISR_ORE  ((uint32_t)0x00000008) /*!< OverRun Error */

USART_ISR_RXNE ((uint32_t)0x00000020) /*!< Read Data Register Not Empty */

I try to set USART3->ISR = 0. but it does not work.

  1. How to clear these bits?
  2. Any bits to be cleared in void HAL_UART_RxCpltCallback (UART_HandleTypeDef *huart) function

Jiannong

Tesla DeLorean
Guru
September 1, 2022

I believe all of this is covered in the Reference Manual for the parts

char GetChar(void)
{
 if (USART_RS232->ISR & USART_ISR_ORE) // Overrun Error
 USART_RS232->ICR = USART_ICR_ORECF;
 if (USART_RS232->ISR & USART_ISR_NE) // Noise Err
 USART_RS232->ICR = USART_ICR_NCF;
 if (USART_RS232->ISR & USART_ISR_FE) // Framing Error
 USART_RS232->ICR = USART_ICR_FECF;
 
 if ((USART_RS232->ISR & USART_ISR_RXNE) == 0)
 return(0);
 
 return((char)(USART_RS232->RDR & 0xFF));
} 

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Jiannong Zhou
Associate III
September 1, 2022

Hi Tesla,

Thank you so much for your detailed information. I will try it out.

Jiannong

Jiannong Zhou
Associate III
September 3, 2022

Hi Tesla,

I tested it to clear the error bits - USART_ISR_ORE and USART_ISR_RXNE. it can run over night. No problems.

I have two questions,

  1. What does cause USART_ISR_ORE - over run error?
  2. Is it correct that USART_ISR_RXNE error is caused by USART_ISR_ORE error?

Jiannong

Tesla DeLorean
Guru
September 3, 2022

RXNE is RX Not Empty, so indicates data available.

O​RE suggests you missed the service window, ie RXNE already signaling and more data arrives with no place to put it.

C​heck that you don't have blocking code in a higher priority interrupt or callbacks.

K​eep handlers very quick/cheap and put them in a group that can preempt slower and less critical ones.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Jiannong Zhou
Associate III
September 11, 2022

Hi Tesla,

Now I cleared these two bits when each interrupt routine calls. At least the communication does nots stop.

I need to do more detailed investigation to find which higher priority interrupt or callbacks to cause this issue.

Thank you so much for your advice.

Thanks,

Jiannong