Skip to main content
danny2
Associate
Aug 31, 2015 3:45 PM UTC
Question

STM32F303 - Changing PWM mode on the fly

Posted on August 31, 2015 at 17:45

Hi,

I use TIM1 PWM in asymmetric mode. I need to switch between 2 software modes : Mode A - CH1/1N asym mode 2, CH3/3N asym mode 2 Mode B - CH1 asym mode 1, CH3 asym mode 2, CH1N/3N off I use HAL for initialization but I need the transition between these 2 modes to be as quick as possible (and HAL is troubling me a bit) : Transition to mode A :

// disable PWMs
htim1.Instance->CCER &= ~( TIM_CCER_CC1E
| TIM_CCER_CC1NE
| TIM_CCER_CC3E
| TIM_CCER_CC3NE );
htim1.Instance->BDTR&= ~TIM_BDTR_MOE;
htim1.Instance->CR1 &= ~TIM_CR1_CEN;
// configure
htim1.Instance->BDTR |= TIM_BDTR_DTG & TIM1_FREQ / DEAD_TIME_INVERSE;
htim1.Instance->CCMR1 |= TIM_CCMR1_OC1M & TIM_OCMODE_ASSYMETRIC_PWM2
| TIM_CCMR1_OC2M & TIM_OCMODE_ASSYMETRIC_PWM2 << 8;
htim1.Instance->CCR1= 0;
htim1.Instance->CCR2= htim1.Instance->ARR;
htim1.Instance->CCR3= x;
htim1.Instance->CCR4= y;
// enable PWMs
htim1.Instance->CCER |= TIM_CCER_CC1E
| TIM_CCER_CC1NE
| TIM_CCER_CC3E
| TIM_CCER_CC3NE;
htim1.Instance->BDTR|= TIM_BDTR_MOE;
htim1.Instance->CR1 |= TIM_CR1_CEN;

Transition to mode B :

// disable PWMs
htim1.Instance->CCER &= ~( TIM_CCER_CC1E
| TIM_CCER_CC1NE
| TIM_CCER_CC3E
| TIM_CCER_CC3NE );
htim1.Instance->BDTR&= ~TIM_BDTR_MOE;
htim1.Instance->CR1 &= ~TIM_CR1_CEN;
// configure
htim1.Instance->BDTR &= ~TIM_BDTR_DTG; 
// remove deadtime
htim1.Instance->CCMR1 |= TIM_CCMR1_OC1M & TIM_OCMODE_ASSYMETRIC_PWM1
| TIM_CCMR1_OC2M & TIM_OCMODE_ASSYMETRIC_PWM1 << 8;
htim1.Instance->CCR1= 300;
htim1.Instance->CCR2= 0;
htim1.Instance->CCR3= htim1.Instance->ARR;
htim1.Instance->CCR4= htim1.Instance->ARR - htim1.Instance->CCR1;
// enable PWMs
htim1.Instance->CCER |= TIM_CCER_CC1E
| TIM_CCER_CC3E;
htim1.Instance->BDTR|= TIM_BDTR_MOE;
htim1.Instance->CR1 |= TIM_CR1_CEN;

The problem is : mode A looks ok, but when in mode B channel 1 stays in asymmetric PWM mode 2. I tried a lot of things, including trying similar code with HAL_PWM_Start/Stop and other things. Sometimes channel 1 switches to asym mode 1 as needed, but it looks like chance. One more thing : I initialize all channels in PWM asym mode 2 with HAL. But when I initialize CH1/2 in mode 1 and CH3/4 in mode 2, it works better, I don't know why. Thanks in advance.
    This topic has been closed for replies.

    2 replies

    waclawek.jan
    Super User
    Aug 31, 2015 8:19 PM UTC
    Posted on August 31, 2015 at 22:19

    htim1.Instance->CCMR1 |= TIM_CCMR1_OC1M & TIM_OCMODE_ASSYMETRIC_PWM1
    | TIM_CCMR1_OC2M & TIM_OCMODE_ASSYMETRIC_PWM1 << 8;

    The

    TIM_CCMR1_OC1M

    bits are already all set from being set for PWM2 in previous step. You perhaps wanted to use = rather than |=. Also, aren't the channel3 bits in CCMR2? (I personally woldn't mix in the constants defined in CUBE (e.g.

    TIM_OCMODE_ASSYMETRIC_PWM1

    ) and would stick to the constants defined in the basic CMSIS device header stm32f3xx.h, but that's me.) JW
    danny2
    danny2Author
    Associate
    Sep 1, 2015 6:47 AM UTC
    Posted on September 01, 2015 at 08:47

    Indeed, the problem was the operator...

    Thank you very much ! I feel a bit stupid x)