Skip to main content
aman sehgal
Associate
Jun 20, 2018 3:50 AM UTC
Solved

stm32f303 ADC continuous conversion mode multi-channel does not auto start new sequence

Posted on June 20, 2018 at 05:50

I am using a STM32F303v with 2 ADC regular channels in cotinuous mode with a DMA and would like continuous conversion to take place in order to enable a stream of data.

Base on the setup of my DMA and ADC below, I am unable to perform continuous conversion. On further debugging, I found that the very first conversion is successful and then the ADSTART bit is set back to 0. If I manually set ADSTART=1, the conversion starts, DMA does the transfer when it finishes and then ADSTART goes back to 0. Please help.

    DMAy_x

=

DMA1_Channel1;

    DMA_InitStructure.

DMA_M2M

=

DMA_M2M_Disable;

    DMA_InitStructure.

DMA_MemoryBaseAddr

=

(

uint32_t

)dest;

    DMA_InitStructure.

DMA_DIR

=

DMA_DIR_PeripheralSRC;

    DMA_InitStructure.

DMA_Mode

=

DMA_Mode_Circular;

    DMA_InitStructure.

DMA_Priority

=

DMA_Priority_High;

    DMA_InitStructure.

DMA_PeripheralDataSize

=

DMA_PeripheralDataSize_HalfWord;

    DMA_InitStructure.

DMA_MemoryDataSize

=

DMA_MemoryDataSize_HalfWord;

    DMA_InitStructure.

DMA_MemoryInc

=

DMA_MemoryInc_Enable;

    DMA_InitStructure.

DMA_PeripheralInc

=

DMA_PeripheralInc_Disable;

    DMA_InitStructure.

DMA_BufferSize

=

 2;

// in data unit

    DMA_InitStructure.

DMA_PeripheralBaseAddr

=

(

uint32_t

)

&

ADCx->

DR

;

    

DMA_Init

(DMAy_x,

&

DMA_InitStructure);

    

DMA_Cmd

(DMAy_x, ENABLE);

    ADCx = ADC1;

    ADC_Cmd

(ADCx, DISABLE);

    

while

(ADCx->

CR

&

ADC_CR_ADEN);

    

ADC_DeInit

(ADCx);

    ADC_InitTypeDef ADC_InitStructure;

    

ADC_StructInit

(

&

ADC_InitStructure);

    ADC_InitStructure.

ADC_ContinuousConvMode

=

ENABLE;

    ADC_InitStructure.

ADC_DataAlign

=

ADC_DataAlign_Right;

    ADC_InitStructure.

ADC_Resolution

=

ADC_Resolution_12b;

    ADC_InitStructure.

ADC_NbrOfRegChannel

=

 2;

    ADC_InitStructure.

ADC_ExternalTrigEventEdge

=

ADC_ExternalTrigEventEdge_None;

    ADC_InitStructure.

ADC_ExternalTrigConvEvent

=

ADC_ExternalTrigConvEvent_0;

    ADC_InitStructure.

ADC_OverrunMode

=

ENABLE;

    ADC_InitStructure.

ADC_AutoInjMode

=

DISABLE;

    

    

ADC_Init

(ADCx,

&

ADC_InitStructure);

    

// Set up ADC channels

    

for

(

uint16_t

i

=

0

; i

<

nPins;

++

i)

    {

        

// make them regular channels with rank i +1, sample time is 19 ADC cycles

        

ADC_RegularChannelConfig

(ADCx, PIN_MAP[pinNames[i]].

adcChannel

, i

+

1

, ADC_SAMPLE_TIME); 

    }

    ADC_DMAConfig

(ADCx, ADC_DMAMode_Circular);

    ADC_DMACmd

(ADCx, ENABLE);

    

// Enable everything

    

ADC_Cmd

(ADCx, ENABLE);

    while

(

!

(

ADC_GetFlagStatus

(ADCx, ADC_FLAG_RDY)));

    ADC_StartConversion

(ADCx);

#stm32f303 #dma-adc-stm32f303 #stm32f303-adc
This topic has been closed for replies.
aman sehgal
aman sehgalBest answer
Associate
Jun 20, 2018 7:03 PM UTC
Posted on June 20, 2018 at 21:03

The bug was in this line

ADC_InitStructure.ADC_ContinuousConvMode = ENABLE;

It should be

ADC_InitStructure.ADC_ContinuousConvMode = ADC_ContinuousConvMode_Enable;

1 reply

aman sehgal
aman sehgalAuthorBest answer
Associate
Jun 20, 2018 7:03 PM UTC
Posted on June 20, 2018 at 21:03

The bug was in this line

ADC_InitStructure.ADC_ContinuousConvMode = ENABLE;

It should be

ADC_InitStructure.ADC_ContinuousConvMode = ADC_ContinuousConvMode_Enable;