STM32F303 actual samples per second from ADC
Hello! I am trying to figure out my sampling time from my ADC. The setup i have:
A number of ADC:s setup with a DMA. All ADC has the same sample time, set to 19.5 ADC cycles. All ADC is 12 bit, so from my understanding, we have 19.5 + 12.5 = 32 ADC cycles so far. The ADCCLK is set to 64MHz.
If I understood the Reference manual correctly, this would mean the total conversion time for the ADC is: (1/64MHz) * 32 = 0.5 microseconds. If this value is correct(Correct me if its wrong), then would this mean that the DMA interrupt would fire this often, or am I wrong? I am more interested in knowing how many samples per second I could expect realistically with my setup. I imagine this would also depend on the size of my interrupt, but we don't have to be that precise.
Thank you in advance, and let me know if any more info is needed!