Skip to main content
hilwan
Associate III
February 10, 2014
Question

STM32F3 USB

  • February 10, 2014
  • 11 replies
  • 2246 views
Posted on February 10, 2014 at 17:48

Hello,

I've downloaded the custom-hid program on the STM32F3 Discovery . I've alsoinstalled the usb hid demonstrator. But it doesn't recognise any 'USBHID target'. How can I make the host talkto my board? Will it happen automatically if the program is fine when Irun it or should I have to make some change in Windows 8 settings?

I'm using KeilµVision4.

Thanks in advance.

    This topic has been closed for replies.

    11 replies

    hilwan
    hilwanAuthor
    Associate III
    February 12, 2014
    Posted on February 12, 2014 at 16:37

    STM32F3 USB

    Hello,

    I've downloaded the custom-hid program on the STM32F3 Discovery . I've alsoinstalled the usb hid demonstrator. But it doesn't recognise any 'USBHID target'. How can I make the host talkto my board? Will it happen automatically if the program is fine when Irun it or should I have to make some change in Windows 8 settings?

    I'm using KeilµVision4.

    Thanks in advance.

    0690X0000060MnyQAE.gif

    Tesla DeLorean
    Guru
    February 12, 2014
    Posted on February 12, 2014 at 18:22

    Windows 8 will not run ''Unsigned Drivers'' unless specifically overridden to do so.

    http://www.trickday.com/2012/09/how-to-install-unsigned-drivers-in-windows-8/

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    hilwan
    hilwanAuthor
    Associate III
    February 12, 2014
    Posted on February 12, 2014 at 18:50

    Think you clive1 for your replay. In fact, i used the Custom_Hid of STM32303C_EVAL into my Discovery F3 with any configurations change. This would be the problem ? 

    When i tried the USB-FS-Device Mouse example for the DiscF3, i can see it with the USB HID demonstrator.

     Windows 8 will not run ''Unsigned Drivers'': I did it when i want to install the St-link module. 

    Tesla DeLorean
    Guru
    February 12, 2014
    Posted on February 12, 2014 at 19:11

    I don't have any specific understanding of HID devices, I would however recommend XP or Win7 as a platform to do initial experimentation under, Win8 will just compound any headaches you are having.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    hilwan
    hilwanAuthor
    Associate III
    February 12, 2014
    Posted on February 12, 2014 at 19:31

    I tried also with XP but the same problem. I m making certain modifications in the sources code to adapt them with the F3 discovery, i will see if it would change something.

    hilwan
    hilwanAuthor
    Associate III
    February 17, 2014
    Posted on February 17, 2014 at 12:23

    Hello again,

    I've ported the Custom HID Demo of the STM32303C_EVAL to the Discovery but my board can't be recognized, i tried it with different OS(wind8, wind7, XP) but always the same problem.

    The mouse example works fine.

    Should i install a specific driver for this stuff ?

    Thanks in advance  

    chen
    Associate II
    February 17, 2014
    Posted on February 17, 2014 at 13:41

    Hi

    ''The mouse example works fine.''

    ''I've ported the Custom HID Demo of the STM32303C_EVAL to the Discovery''

    If the original demo works - then the USB HID driver on the Host is OK.

    The problem is with your ''Custom HID demo'' !

    Look at the differences between the working example HID demo and your custom HID demo.

    hilwan
    hilwanAuthor
    Associate III
    February 18, 2014
    Posted on February 18, 2014 at 18:24

    Ok,sung.chen_chung, thanks for your answer, i'll try to fix that.

    But, i still have a question about VirtualCOMPort example of STM32_USB-FS-Device_Lib_V4.0.0. in Readme file it says that:

    This demo is using two different methods for the IN and OUT transfers in order 

    to manage the data rate difference between USB and USART buses:

     - OUT transfers (from Host to Device):

         When a packet is received from the host on the OUT pipe (EP3), the Endpoint

         callback function is called when the transfer is complete and all the received

         data are then sent through USART peripheral in polling mode. This allows all

         incoming OUT packets to be NAKed till the current packet is completely transferred

         through the USART interface.

     

     - IN transfers (from Device to Host):

         For IN data, a large circular buffer is used. USART and USB respectively write

         and read to/from this buffer independently.

         USART RXNE interrupt is used to write data into the buffer. This interrupt 

         has the highest priority, which allows to avoid overrun and data loss conditions.

         USB IN endpoint (EP1) is written with the received data into the SOF interrupt 

         callback. 

    I can't find the routines that handles this. There is only the function that handles EVAL_COM1 global interrupt request.

    marco
    Visitor II
    May 31, 2014
    Posted on May 31, 2014 at 16:47

    I have also the same problem .. but under win7-64.

    I cannot see any HID device. What i can do?

    marco
    Visitor II
    May 31, 2014
    Posted on May 31, 2014 at 16:58

    In the system I can see the new device like USB device input

    but inside of USB Hid Dem. I cannot see it:

    Thanks in advance.