Skip to main content
dmytro
Associate
September 22, 2013
Question

STM32F3 Timer3 and Timer4 as PWM

  • September 22, 2013
  • 4 replies
  • 1371 views
Posted on September 22, 2013 at 22:46

Hi,

 i use a STM32f3discovery evaluation board and trying to generate 6 PWM signals. For this purpose i have choosen Timers 3 and 4. As base project i use a Demo project. (The project demonstrates a sensors functionality) Initialisation code for timers is following:

void Timer_Config(void){

  RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA , ENABLE);

  RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM3, ENABLE);   

  RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM4, ENABLE);   

  //Timer4

  GPIO_PinAFConfig(GPIOA, GPIO_PinSource11, GPIO_AF_10);

  GPIO_PinAFConfig(GPIOA, GPIO_PinSource12, GPIO_AF_10);

  GPIO_PinAFConfig(GPIOA, GPIO_PinSource13, GPIO_AF_10);

 

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_11 | GPIO_Pin_12 | GPIO_Pin_13;

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

  GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

 

  GPIO_Init(GPIOA, &GPIO_InitStructure);

 

  TIM_TimeBaseInitStructure.TIM_Prescaler = 71;

  TIM_TimeBaseInitStructure.TIM_CounterMode = TIM_CounterMode_Up;

  TIM_TimeBaseInitStructure.TIM_Period = 999;

  TIM_TimeBaseInitStructure.TIM_ClockDivision = TIM_CKD_DIV4;

  TIM_TimeBaseInit(TIM4, &TIM_TimeBaseInitStructure);

  //PWM Config on Timer4 CH3

  TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1 ;

  TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;

  TIM_OCInitStructure.TIM_Pulse = 0;

  TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;

  TIM_OC3Init(TIM4, &TIM_OCInitStructure);

  //PWM Config on Timer4 CH2

  TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1 ;

  TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;

  TIM_OCInitStructure.TIM_Pulse = 0;

  TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;

  TIM_OC2Init(TIM4, &TIM_OCInitStructure);

  //PWM Config on Timer4 CH1

  TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1 ;

  TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;

  TIM_OCInitStructure.TIM_Pulse = 0;

  TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;

  TIM_OC1Init(TIM4, &TIM_OCInitStructure);

  TIM_Cmd(TIM4, ENABLE);

 

 

  //Timer3

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4 | GPIO_Pin_6 | GPIO_Pin_7    ;

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

  GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_2MHz;

  GPIO_Init(GPIOA, &GPIO_InitStructure);

 

  GPIO_PinAFConfig(GPIOA, GPIO_PinSource4, GPIO_AF_2);

  GPIO_PinAFConfig(GPIOA, GPIO_PinSource6, GPIO_AF_2);

  GPIO_PinAFConfig(GPIOA, GPIO_PinSource7, GPIO_AF_2);

    //Timer3 Config

  TIM_TimeBaseInitStructure.TIM_Prescaler = 71;

  TIM_TimeBaseInitStructure.TIM_CounterMode = TIM_CounterMode_Up;

  TIM_TimeBaseInitStructure.TIM_Period = 999;

  TIM_TimeBaseInitStructure.TIM_ClockDivision = TIM_CKD_DIV4;

  TIM_TimeBaseInit(TIM3, &TIM_TimeBaseInitStructure);

  //PWM Config on Timer3 CH3

  TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1 ;

  TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;

  TIM_OCInitStructure.TIM_Pulse = 0;

  TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_Low;

  TIM_OC3Init(TIM3, &TIM_OCInitStructure);

  //PWM Config on Timer3 CH2

  TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1 ;

  TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;

  TIM_OCInitStructure.TIM_Pulse = 0;

  TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_Low;

  TIM_OC2Init(TIM3, &TIM_OCInitStructure);

  //PWM Config on Timer3 CH1

  TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1 ;

  TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;

  TIM_OCInitStructure.TIM_Pulse = 0;

  TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_Low;

  TIM_OC1Init(TIM3, &TIM_OCInitStructure);

  TIM_Cmd(TIM3, ENABLE);

}

But if I call this funktion the board stops working. Pin_to_periphery allocation description was taken from DM00058181.pdf dokument form ST site.

Could someone help me make it work?

P.S. I use a USART1 too, it uses pins PA9 and PA10.

#pwm #stm32f3 #timers
This topic has been closed for replies.

4 replies

Tesla DeLorean
Guru
September 22, 2013
Posted on September 22, 2013 at 23:18

But if I call this funktion the board stops working.

How exactly, it crashes, have you used a debugger, where is it crashing?

It has no pulse output? Not surprising Pulse = 0 is OFF, try something like 10, or 500 (50/50)

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Tesla DeLorean
Guru
September 22, 2013
Posted on September 22, 2013 at 23:52

Doesn't PA13 conflict with the debugger SWDAT signal? Need to rethink that perhaps.

// STM32 TIM3/4 PWM (PA11/12,6/7) STM32F3-Discovery - sourcer32@gmail.com
#include ''stm32f30x.h''
/**************************************************************************************/
void RCC_Configuration(void)
{
/* Enable GPIO clock */
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);
/* Enable TIM3/4 clock */
RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM3 | RCC_APB1Periph_TIM4, ENABLE);
}
/**************************************************************************************/
void GPIO_Configuration(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
// Free pins located in STM32F3-Discovery manual, UM1570
// AF located in F302/303 Data Manual (Alternate functions for port A - Table 14, Rev 5)
GPIO_PinAFConfig(GPIOA, GPIO_PinSource11, GPIO_AF_10); // TIM4_CH1
GPIO_PinAFConfig(GPIOA, GPIO_PinSource12, GPIO_AF_10); // TIM4_CH2
// GPIO_PinAFConfig(GPIOA, GPIO_PinSource13, GPIO_AF_10); // TIM4_CH3 (Conflicts with SWDAT debug signal)
// TIM4_CH3 PB8(AF2), PD14(AF2)
// GPIO_PinAFConfig(GPIOA, GPIO_PinSource4, GPIO_AF_2); // TIM3_CH1 !! pick one
GPIO_PinAFConfig(GPIOA, GPIO_PinSource6, GPIO_AF_2); // TIM3_CH1
GPIO_PinAFConfig(GPIOA, GPIO_PinSource7, GPIO_AF_2); // TIM3_CH2
// TIM3_CH3 PB0(AF2), PC8(AF2), PE4 (AF2)
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6 | GPIO_Pin_7 | GPIO_Pin_11 | GPIO_Pin_12;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_2MHz;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_Init(GPIOA, &GPIO_InitStructure);
}
/**************************************************************************************/
void TIM_Configuration(void)
{
TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
TIM_OCInitTypeDef TIM_OCInitStructure;
TIM_TimeBaseStructure.TIM_Prescaler = 72 - 1; // 72 to 1 MHz
TIM_TimeBaseStructure.TIM_Period = 1000 - 1; // 1 MHz to 1 KHz
TIM_TimeBaseStructure.TIM_ClockDivision = TIM_CKD_DIV1;
TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
TIM_TimeBaseInit(TIM4, &TIM_TimeBaseStructure);
TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1;
TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
TIM_OCInitStructure.TIM_Pulse = 1000 / 4; // 25%
TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;
TIM_OC1Init(TIM4, &TIM_OCInitStructure);
TIM_OC2Init(TIM4, &TIM_OCInitStructure);
TIM_OC3Init(TIM4, &TIM_OCInitStructure);
TIM_Cmd(TIM4, ENABLE);
TIM_TimeBaseInit(TIM3, &TIM_TimeBaseStructure);
TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1;
TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
TIM_OCInitStructure.TIM_Pulse = 1000 / 2; // 50%
TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_Low;
TIM_OC1Init(TIM3, &TIM_OCInitStructure);
TIM_OC2Init(TIM3, &TIM_OCInitStructure);
TIM_OC3Init(TIM3, &TIM_OCInitStructure);
TIM_Cmd(TIM3, ENABLE);
}
/**************************************************************************************/
int main(void)
{
RCC_Configuration();
GPIO_Configuration();
TIM_Configuration();
while(1); // Don't want to exit
}

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
dmytro
dmytroAuthor
Associate
September 22, 2013
Posted on September 23, 2013 at 01:14

Wow Thanks Clive,

i will try Your variant tomorrow! I have found that

GPIO_PinAFConfig(GPIOA, GPIO_PinSource13, GPIO_AF_10);

does not work, but could not understood why, thanks for explanation. If I comment the line mentioned above and run timer-initialisation in debug mode (one step per click), the Demo appears to work, (LEDs react on gyro / magnet sensor). But if I ''click'' run it crashes. It isnt actually a crash, the programm simply goes in to HardFault_Handler(void) exeption state. I have an short quastion, can timers conflict with USART? Thanks.
Tesla DeLorean
Guru
September 23, 2013
Posted on September 23, 2013 at 02:56

The pin usage on the STM32F3-DISCO can be located

http://www.st.com/st-web-ui/static/active/en/resource/technical/document/user_manual/DM00063382.pdf

.

The USART shouldn't conflict with anything, internally you can only route one function to each pin, externally you could have other inputs/outputs do conflicting things.

A Hard Fault is more indicative of a missing interrupt service routine, a proper handler will allow you to determine a more precise cause/causes. Check also for corrupting the stack, and accessing memory outside normal bounds.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..