Question
STM32F3 Timer Output Compare Mode
Posted on July 13, 2015 at 04:19
I'm trying to configure TIM2 CH1-4 as per the sample code, and CH2-4 are working at the correct frequency and can be adjusted via the CCR_VAL variables. However CH1 is always toggling at the TIM2_Update frequency and is unaffected by the CCR1_VAL. Is it possible to have CH1 and the TIM2 update trigger at different frequencies?
/**
* @brief Configure the TIM IRQ Handler.
* @param None
* @retval None
*/
void TIMER_Config(void)
{
NVIC_InitTypeDef NVIC_InitStructure;
TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
TIM_OCInitTypeDef TIM_OCInitStructure;
uint16_t PrescalerValue = 0;
/* TIM2 clock enable */
RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE);
/* Enable the TIM2 gloabal Interrupt */
NVIC_InitStructure.NVIC_IRQChannel = TIM2_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
/* -----------------------------------------------------------------------
TIM2 Configuration: Output Compare Timing Mode:
In this example TIM2 input clock (TIM2CLK) is set to 2 * APB1 clock (PCLK1),
since APB1 prescaler is different from 1.
TIM2CLK = 2 * PCLK1
PCLK1 = HCLK / 2
=> TIM2CLK = HCLK = SystemCoreClock
To get TIM2 counter clock at 72 MHz, the prescaler is computed as follows:
Prescaler = (TIM2CLK / TIM2 counter clock) - 1
Prescaler = ((SystemCoreClock) /72 MHz) - 1
CC1 update rate = TIM2 counter clock / CCR1_Val = 1777 Hz
==> Toggling frequency = 888 Hz
C2 update rate = TIM2 counter clock / CCR2_Val = 2649 Hz
==> Toggling frequency = 124 Hz
CC3 update rate = TIM2 counter clock / CCR3_Val = 518 Hz
==> Toggling frequency = 2659 Hz
CC4 update rate = TIM2 counter clock / CCR4_Val = 1059 Hz
==> Toggling frequency = 595 Hz
Note:
SystemCoreClock variable holds HCLK frequency and is defined in system_stm32f3xx.c file.
Each time the core clock (HCLK) changes, user had to call SystemCoreClockUpdate()
function to update SystemCoreClock variable value. Otherwise, any configuration
based on this variable will be incorrect.
----------------------------------------------------------------------- */
/* Compute the prescaler value */
PrescalerValue = (uint16_t) ((SystemCoreClock) / 64000000) - 1;
/* Time base configuration */
TIM_TimeBaseStructure.TIM_Period = 65535;
TIM_TimeBaseStructure.TIM_Prescaler = 0;
TIM_TimeBaseStructure.TIM_ClockDivision = 0;
TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
TIM_TimeBaseInit(TIM2, &TIM_TimeBaseStructure);
/* Prescaler configuration */
TIM_PrescalerConfig(TIM2, PrescalerValue, TIM_PSCReloadMode_Immediate);
/* Init TIM_OCInitStructure */
TIM_OCStructInit(&TIM_OCInitStructure);
/* Output Compare Timing Mode configuration: Channel1 */
TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_Timing;
TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
TIM_OCInitStructure.TIM_Pulse = CCR1_Val;
TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;
TIM_OC1Init(TIM2, &TIM_OCInitStructure);
TIM_OC1PreloadConfig(TIM2, TIM_OCPreload_Disable);
/* Output Compare Timing Mode configuration: Channel2 */
TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
TIM_OCInitStructure.TIM_Pulse = CCR2_Val;
TIM_OC2Init(TIM2, &TIM_OCInitStructure);
TIM_OC2PreloadConfig(TIM2, TIM_OCPreload_Disable);
/* Output Compare Timing Mode configuration: Channel3 */
TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
TIM_OCInitStructure.TIM_Pulse = CCR3_Val;
TIM_OC3Init(TIM2, &TIM_OCInitStructure);
TIM_OC3PreloadConfig(TIM2, TIM_OCPreload_Disable);
/* Output Compare Timing Mode configuration: Channel4 */
TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
TIM_OCInitStructure.TIM_Pulse = CCR4_Val;
TIM_OC4Init(TIM2, &TIM_OCInitStructure);
TIM_OC4PreloadConfig(TIM2, TIM_OCPreload_Disable);
/* TIM Interrupts enable */
TIM_ITConfig(TIM2, TIM_IT_CC1 | TIM_IT_CC2 | TIM_IT_CC3 | TIM_IT_CC4, ENABLE);
/* TIM2 enable counter */
TIM_Cmd(TIM2, ENABLE);
}
/**
* @brief This function handles TIM2 global interrupt request.
* @param None
* @retval None
*/
void TIM2_IRQHandler(void)
{
/* End of pulse- Reset VDDP to 5.0V */
if (TIM_GetITStatus(TIM2, TIM_IT_Update) != RESET)
{
HAL_GPIO_TogglePin(WS2812_PORT, GPIO_Pin_0);
TIM_ClearITPendingBit(TIM2, TIM_IT_Update);
TIM_SetCounter(TIM2, 0);
}
else if (TIM_GetITStatus(TIM2, TIM_IT_CC1) != RESET)
{
TIM_ClearITPendingBit(TIM2, TIM_IT_CC1);
/* LED1 toggling with frequency = 888 Hz */
HAL_GPIO_TogglePin(WS2812_PORT, GPIO_Pin_1);
TIM_SetCompare1(TIM2, capture + CCR1_Val);
}
else if (TIM_GetITStatus(TIM2, TIM_IT_CC2) != RESET)
{
TIM_ClearITPendingBit(TIM2, TIM_IT_CC2);
/* LED2 toggling with frequency = 124 Hz */
HAL_GPIO_TogglePin(WS2812_PORT, GPIO_Pin_2);
capture = TIM_GetCapture2(TIM2);
TIM_SetCompare2(TIM2, capture + CCR2_Val);
}
else if (TIM_GetITStatus(TIM2, TIM_IT_CC3) != RESET)
{
TIM_ClearITPendingBit(TIM2, TIM_IT_CC3);
/* LED3 toggling with frequency = 2659 Hz */
HAL_GPIO_TogglePin(WS2812_PORT, GPIO_Pin_3);
capture = TIM_GetCapture3(TIM2);
TIM_SetCompare3(TIM2, capture + CCR3_Val);
}
else
{
TIM_ClearITPendingBit(TIM2, TIM_IT_CC4);
/* LED4 toggling with frequency = 595 Hz */
HAL_GPIO_TogglePin(WS2812_PORT, GPIO_Pin_4);
capture = TIM_GetCapture4(TIM2);
TIM_SetCompare4(TIM2, capture + CCR4_Val);
}
}