Question
STM32F3 programming flash writing (missing function)
Posted on July 29, 2015 at 15:09
Hello,
Recently I've been trying to configure writing to flash memory in STM32F3 discovery. I'm using STM32CubeMX and System Workbench for STM32. I've read many guides how to do it and example codes so I guess I already have some idea how it should work. However everywhere I look and read, people are using prepared functions like FLASH_Unlock() Lock() etc. Almost the same functions are in HAL library which I'm trying to use but I'm missing one. It is: FLASH_ClearFlag(...) My question is: does HAL libraries contain a substitute for that function (which I unfortunatelly can't find) or I just have to include a certain library to my project and if so, then what library? Regards Dominik O.