Skip to main content
kim
Visitor II
June 21, 2018
Question

STM32F3 Interrupt and timers

  • June 21, 2018
  • 3 replies
  • 883 views
Posted on June 21, 2018 at 10:56

I am running STM32F303VC.

I require an IRQ on GPIOE_Pin_15  ---> TIM2_Channel_1

My typical Frequency range is from 5 Hz - 500Hz

This is required to provide me with a number of ticks between the 2 interrupts.  The result is then passed to TIM3 /100

PreScaler   = Same for both timers

TIM2_Period = 1

TIM3_Period = Result / 100

TIM3 then provides me with 100 points between the original to trigger other events an certain points.

The problem I am having is the IRQ_Handlers do not get triggered.

I have monitored the GPIO_Pin_15 through a while loop and confirm this is toggling, however TIM2 doe not update TIM3 and TIM3 does NOT output either.

I can provide my Main.C file if you email me

mailto:kim@accesssecurity.co.nz

#stm32f3 #timer-interrupt
This topic has been closed for replies.

3 replies

waclawek.jan
Super User
June 21, 2018
Posted on June 21, 2018 at 17:01

The problem I am having is the IRQ_Handlers do not get triggered.

Read back the content of relevant GPIO and TIM (and NVIC) registers and

- check if AF is set for given pin in GPIO_MODER

- check if the proper AF is selected in GPIO_AFRL/AFRH

- check if input capture is set in TIMx_CCMRy

- check if channel enabled in TIMx_ENR

- check if interrupt for that channel enabled in TIMx_DIER

- check if interrupt for that timer is enabled in NVIC

- check if the ISR name matches that in the vector/startup file(keep in mind name mangling if you compile as C++) (check in disassembled binary perhaps)

JW

henry.dick
Associate II
June 21, 2018
Posted on June 21, 2018 at 17:09

'

The problem I am having is the IRQ_Handlers do not get triggered.'

yeah. but the problem isn't with your code. so look somewhere else, please.

waclawek.jan
Super User
June 21, 2018
Posted on June 21, 2018 at 20:02

Indeed, there's no such AF on that pin... I didn't realize the OP didn't care to check...

JW