Skip to main content
pierric
Associate
June 4, 2013
Question

STM32F3 Discovery / STM32F303VC 5V tolerant IO

  • June 4, 2013
  • 4 replies
  • 1585 views
Posted on June 04, 2013 at 18:38

Good afternoon,

I'm a student working on a robotic project using a STM32F3 discovery evaluation board.

I read that there are several IO that are 5 volts tolerant among all IOs the board have.

The issue is that I can't find which outputs are 5 volts tolerant in the chip.

I search several ST documentations, the web and the library...

Did anyone found this information ? Any help will be appreciated !

Sincerly,

P.G

#stm32 #discovery
    This topic has been closed for replies.

    4 replies

    Tesla DeLorean
    Guru
    June 4, 2013
    Posted on June 04, 2013 at 19:24

    None of the pins are going to physically output 5V.

    You'll have to check if the VOL/VOH levels output from the STM32 via it's primary supply are adequate.

    To get to 5V you'll need to program a pin in OD (Open Drain) mode, and use an external pull-up resistor to a 5V supply. These would need to be the same FT (Five volt Tolerant) pins listed in the data manual.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    pierric
    pierricAuthor
    Associate
    June 4, 2013
    Posted on June 04, 2013 at 19:33

    Thank you for the answer, but the issue is different :

    I should have precised that the aim is to have 5 volts input without burning some inputs, as it seems that only some of theses inputs are 5 volts tolerant.

    I have 2 encoders that only works with TTL logic levels and therefore give me 5 volts signals to be analysed.

    Tesla DeLorean
    Guru
    June 4, 2013
    Posted on June 04, 2013 at 19:38

    And these pins are identified in the manual for the part? No?

    http://www.st.com/web/catalog/mmc/FM141/SC1169/SS1576/LN1531/PF252054

    http://www.st.com/st-web-ui/static/active/en/resource/technical/document/datasheet/DM00058181.pdf

    This doesn't preclude you from adding external level conversion logic either, or resistor dividers.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    pierric
    pierricAuthor
    Associate
    June 4, 2013
    Posted on June 04, 2013 at 20:40

    Thank you for the links, I already had read this documentation but I didn't found the information... and it is available in the pinout and pin description chapter.

    On page 10, we learn there are 45 ''normal'' TC/TTa GPIO and 42 ''5 volt tolerant'' FT/FTf GPIO.

    Later on pages 36 and following, there is all the information I needed.

    Many thanks, best regards,

    P.G