Skip to main content
mattfox
Associate III
Jun 18, 2013 6:47 PM UTC
Question

STM32F3 Discovery Running Code

Posted on June 18, 2013 at 20:47

This is a really basic question, but I'm just starting out on this board. I've been able to run programs through the Debug interface of ST-Link in Eclipse.  Now I'm trying to get printf working with USART2, so I need the miniB cable attached to the breakout board I'm attaching to the board pins for Tx and Rx which means I can't really run through Debug mode because ST-Link needs the MiniB cable attached only to the ST-Link USB and not to the breakout board.  

I was wondering how to run a program that is loaded onto flash memory without using Debug mode.  I'm assuming there should be some easy way to run a program via one of the buttons or something, but i'm pretty clueless.  The board is being powered through the breakout board I'm using.  

Thanks for the help in advance!
    This topic has been closed for replies.

    2 replies

    Tesla DeLorean
    Guru
    Jun 18, 2013 7:18 PM UTC
    Posted on June 18, 2013 at 21:18

    The question is a bit awkwardly stated.

    You don't have to run through the debugger, you write the code to flash, it runs when power is applied, the power is derived from the ST-Link USB interface, and also shares the 8 MHz crystal from the F103 device.

    I know nothing of your break-out board or it's requirements, or why that precludes you from powering the ST-Link USB connector.

    Depending on the tool chain piping printf() data out the USART requires replacement of putchar(), or other semi-hosting changes. On Keil it's also reasonably easy to pipe the data via the SWV/SWO interface into the debugger, removing the need to use a USART for debug output.
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    mattfox
    mattfoxAuthor
    Associate III
    Jun 19, 2013 8:08 PM UTC
    Posted on June 19, 2013 at 22:08

    Yeah, I realize now that I worded the questions awkwardly because it just runs once it gets powered.  

    Turns out that while setting up USART I hadn't installed the serial port driver so I assumed it wasn't running when, in fact, I just wasn't getting the data.  

    Thanks for the help!!