Question
STM32F3 Discovery - ADC Offset
Posted on July 10, 2013 at 23:04
I'm working on getting the ADC fully integrated with the rest of my code. When I'm testing out my ADC, however, I keep getting an output of about 300-400 from ADC1->DR when I'm inputting a voltage of 0 to the pin. I have six pins configured for the ADC, and all of them exhibit this behavior. Furthermore, if I put in a voltage of 2.9 or higher, I am maxed out at 4095. Does anyone know why the values between 2.9 and 3.3 don't register a difference in output?
One of my speculated reasons for this behavior is that I have stopped waiting for the hardware to tell me that it is done with calibration (for reasons I stated in another thread recently). I am wondering if this could be a product of incomplete calibration. I'm not sure what really happens during ADC calibration, and if someone knows, I'd love to have a quick description.One other question that I have is whether this offset would be generalized across devices. I'm currently working with just one discovery board, but I'm planning on putting this chip on a new board, and i'd like to know if I can expect this sort of offset, or if this is a product of this just chip. Thanks so much for any help you can provide! I really appreciate it