Skip to main content
milanmeh
Visitor II
July 25, 2015
Question

STM32F3 16-bit SD ADC resolution in Single Ended mode.

  • July 25, 2015
  • 1 reply
  • 562 views
Posted on July 25, 2015 at 13:19

I would like to know what is the maximal resolution of 16-bit Sigma Delta ADC on STM32F3 line of microcontrollers when used in single ended mode? Can it achieve full 16-bit resolution, 0-65535, in SE mode?

    This topic has been closed for replies.

    1 reply

    Amel NASRI
    ST Technical Moderator
    July 30, 2015
    Posted on July 30, 2015 at 17:16

    Hi laketic.milan.001,

    The SDADC in STM32F37x devices supports 2 single-ended modes:

    1. Single-ended offset mode: is like differential mode with minus pin grounded, so in this mode we lost half of the range and the resolution is 15 bits.
    2. Single-ended zero reference mode: the full positive/negative dynamic range is maintained so the resolution is 16 bits.
    You may get more details on these 2 modes in

    http://www.st.com/st-web-ui/static/active/en/resource/technical/document/reference_manual/DM00041563.pdf

    .

    -Mayla-

    To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.