Skip to main content
w21685
Associate II
Oct 23, 2016 6:09 PM UTC
Question

STM32F2xx Flash memory partial erasing?

Posted on October 23, 2016 at 20:09

Hello,

Would it be possible to erase the flash memory partially before writing data ?

It takes a long time to erase 1sector base. (128kByte or 64kByte)

If possible, could you some advice how to apply?

Thanks.

    This topic has been closed for replies.

    4 replies

    Tesla DeLorean
    Guru
    Oct 23, 2016 6:44 PM UTC
    Posted on October 23, 2016 at 20:44

    Create a gap in your firmware image so you use the 16kb sectors.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    w21685
    w21685Author
    Associate II
    Oct 24, 2016 2:25 PM UTC
    Posted on October 24, 2016 at 16:25

    Thank you for your reply.

    But I don't understand what you mentioned.

    If possible, could you be more specific?

    Thanks.

    Tesla DeLorean
    Guru
    Oct 24, 2016 4:10 PM UTC
    Posted on October 24, 2016 at 18:10

    Break the Load Region for your firmware into TWO separate areas using your Linker Script or Scatter File.

    ie

    Region 1 0x08000000..0x080003FFF 16KB

    Region 2 0x08010000..0x0800FFFFF 1MB-64KB

    Then you will have THREE 16KB sectors at 0x08004000, 0x08008000 and 0x0800C000 which will erase faster

    Alternative create TWO firmwares, a loader that starts at 0x08000000 and an application that starts at 0x08010000

    Review the IAP examples

    Review your tool chain documentation

    The sectors have a defined size, and erase times, you can't do a partial erase. You can write multiple instances of the same structure back-to-back in flash, and then find the most recent, a concept call Journalling. Here you only need to erase when you consume all available space, or you can ping-pong between two flash sectors

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    w21685
    w21685Author
    Associate II
    Oct 24, 2016 6:13 PM UTC
    Posted on October 24, 2016 at 20:13

    Thanks. I will try it.