Skip to main content
ho_it
Associate III
December 8, 2014
Question

STM32F2xx detect CAN speed mismatch when receiving data

  • December 8, 2014
  • 0 replies
  • 329 views
Posted on December 08, 2014 at 05:46

I am using STM32F2xx, and CAN1. I using NVID for the CAN data

I have configured my firmware to receive CAN data at 1Mbps, but how can I detect if the receive CAN speed rate is not 1Mbps? so I can display in my LED that the CAN speed is different

Ex: I cant get any CAN data event in the interupt at 500kbps, is there anyway I can get the CAN speed mismatch event?
    This topic has been closed for replies.