STM32F207ZGT6 – Using an external 8 MHz oscillator without HSE Bypass mode
Hello,
Following an investigation into an intermittent USB DFU issue on our STM32F207ZGT6 boards, I would like to clarify one point regarding the use of an external clock oscillator with the STM32F207.
In our previous discussion (STM32F207ZGT6 – Differences Between Silicon Revisions and DFU Failure), ST confirmed that the STM32F207 HSE stage can operate with an external oscillator even when HSE Bypass mode is not enabled. The external clock pulses are detected, HSE ready is set, and the ROM bootloader can then operate normally.
We have successfully tested this configuration on our hardware:
-
External 8 MHz oscillator output connected directly to OSC_IN.
-
OSC_OUT left unconnected.
-
No changes to the existing application firmware or STM32 clock configuration.
Our existing application firmware configures the HSE using:
RCC_HSE_ON
HSE Bypass mode is therefore not enabled.
My question is whether this configuration is also supported for the user application.
Can the STM32F207 reliably operate with an external 8 MHz oscillator connected to OSC_IN and OSC_OUT left unconnected, while the application continues to configure the HSE using RCC_HSE_ON?
Or is HSE Bypass mode strictly required for reliable operation of the user application, even though the hardware HSE stage can apparently work without it?
This is a critical point for us because we have an existing installed base of products sharing the same firmware. We cannot introduce a different firmware version for the new hardware revision, nor can we update the firmware already deployed in the field.
Any new hardware design must therefore remain fully compatible with our existing application firmware.
Could you please confirm whether this operating mode is supported and reliable, and whether there are any limitations or precautions we should consider?
Thank you for your help.
Best regards,