Skip to main content
kkawula
Associate II
July 14, 2014
Question

STM32F207VE problem with RTC

  • July 14, 2014
  • 0 replies
  • 544 views
Posted on July 14, 2014 at 15:38

Hello

I’m using

https://kelectronics.eu/usvn/repos/EnvRegulator/trunk/Firmware/Env_Regulator/STM32F207VE.ld

and I have problems with RTC. I can configure it and write initialization data (time and date) and RTC seems to work ok. Time counter counts up every second but at 23:59:59 it

does not reset but still counts up (24:00:00, 24:00:01 … and so on!)

The second problem is when I write data using function:

RTC_SetDate(RTC_Format_BIN, &RTC_DateStructure)

And after checking RTC registers with JTAG I can see new data inside them. But every time when I call function RTC_GetDate(RTC_Format_BIN, &RTC_DateStructure) it returns old settings..:(

Only after reset RTC_GetDate(RTC_Format_BIN, &RTC_DateStructure) returns valid date, but when I set new date situation repeats….

Bellow my initialization code:

/** 
* @brief Configure the RTC peripheral by selecting the clock source. 
* @param None 
* @retval None 
*/ 
void RTC_ConfigX(void) 
{ 
#if (_USE_RTC_) 
{ 
RTC_InitTypeDef RTC_InitStructure; 
RTC_TimeTypeDef RTC_TimeStructure; 
/* Enable the PWR clock */ 
RCC_APB1PeriphClockCmd(RCC_APB1Periph_PWR, ENABLE); 
/* Allow access to RTC */ 
PWR_BackupAccessCmd(ENABLE); 
#if(RTC_CLOCK_SOURCE_LSI) /* LSI used as RTC source clock*/ 
/* The RTC Clock may varies due to LSI frequency dispersion. */ 
/* Enable the LSI OSC */ 
RCC_LSICmd(ENABLE); 
/* Wait till LSI is ready */ 
while(RCC_GetFlagStatus(RCC_FLAG_LSIRDY) == RESET) 
{ 
} 
/* Select the RTC Clock Source */ 
RCC_RTCCLKConfig(RCC_RTCCLKSource_LSI); 
SynchPrediv = 0xFF; 
AsynchPrediv = 0x7F; 
debug_printf(_LVL_5, ''RTC_Config LSI clock type setup\n''); 
#elif(RTC_CLOCK_SOURCE_LSE) /* LSE used as RTC source clock */ 
/* Enable the LSE OSC */ 
RCC_LSEConfig(RCC_LSE_ON); 
/* Wait till LSE is ready */ 
while (RCC_GetFlagStatus(RCC_FLAG_LSERDY) == RESET) 
{ 
} 
/* Select the RTC Clock Source */ 
RCC_RTCCLKConfig(RCC_RTCCLKSource_LSE); 
SynchPrediv = 0xFF; 
AsynchPrediv = 0x7F; 
debug_printf(_LVL_5, ''RTC_Config LSE clock type setup\n''); 
#else 
#error Please select the RTC Clock source inside the main.c file 
#endif /* RTC_CLOCK_SOURCE_LSI */ 
/* Enable the RTC Clock */ 
RCC_RTCCLKCmd(ENABLE); 
/* Wait for RTC APB registers synchronisation */ 
RTC_WaitForSynchro(); 
/* Write to the first RTC Backup Data Register */ 
RTC_WriteBackupRegister(RTC_BKP_DR0, FIRST_DATA); 
/* Set the Time */ 
RTC_TimeStructure.RTC_Hours = 0x00; 
RTC_TimeStructure.RTC_Minutes = 0x00; 
RTC_TimeStructure.RTC_Seconds = 0x00; 
/* Set the Date */ 
/* Calendar Configuration */ 
RTC_InitStructure.RTC_AsynchPrediv = AsynchPrediv; 
RTC_InitStructure.RTC_SynchPrediv = SynchPrediv; 
RTC_InitStructure.RTC_HourFormat = RTC_HourFormat_24; 
RTC_Init(&RTC_InitStructure); 
/* Set Current Time and Date */ 
RTC_SetTime(RTC_Format_BIN, &RTC_TimeStructure); 
RTC_SetCompilationDate(); 
/* Backup SRAM ***************************************************************/ 
/* Enable BKPRAM Clock */ 
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_BKPSRAM, ENABLE); 
/* Enable the Backup SRAM low power Regulator to retain it's content in VBAT mode */ 
PWR_BackupRegulatorCmd(ENABLE); 
/* Wait until the Backup SRAM low power Regulator is ready */ 
while (PWR_GetFlagStatus(PWR_FLAG_BRR) == RESET) 
{ 
} 
/* RTC Backup Data Registers **************************************************/ 
/* Write to RTC Backup Data Register */ 
RTC_WriteBackupRegister(RTC_BKP0R, FIRST_DATA); //store first data to bacup reg 
} 
#endif 
} 
/** 
* @brief Main RTC config function 
* First it chcecks if rtc was configured and is maintain by external 
* bacup voltage source 
* If not RTC_ConfigX is executed 
* @param None 
* @retval None 
*/ 
RTC_ConfigState_t RTC_Config(void) 
{ 
RTC_ConfigState_t RTC_ConfigState; 
#if(_USE_RTC_) 
EXTI_InitTypeDef EXTI_InitStructure; 
NVIC_InitTypeDef NVIC_InitStructure; 
//read first bacup register and check it has test data valid 
if (RTC_ReadBackupRegister(RTC_BKP_DR0) != FIRST_DATA) 
{ 
RTC_ConfigX(); 
debug_printf(_LVL_5,''RTC jeszcze nie konfigurowane\r\n''); 
RTC_ConfigState=RTC_ConfigState_FirstConfig; 
} 
else 
{ 
debug_printf(_LVL_5,''RTC już raz włącznone i skonfigurowane\r\n''); 
RTC_ConfigState=RTC_ConfigState_NoNeedToconfig; 
/* Enable the PWR clock */ 
RCC_APB1PeriphClockCmd(RCC_APB1Periph_PWR, ENABLE); 
/* Allow access to RTC */ 
PWR_BackupAccessCmd(ENABLE); 
/* Wait for RTC APB registers synchronisation */ 
RTC_WaitForSynchro(); 
/* Clear the RTC Alarm Flag */ 
RTC_ClearFlag(RTC_FLAG_ALRAF); 
/* Clear the EXTI Line 17 Pending bit (Connected internally to RTC Alarm) */ 
EXTI_ClearITPendingBit(EXTI_Line17); 
/* Enable the PWR APB1 Clock Interface */ 
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_BKPSRAM, ENABLE); 
} 
///-- Configure RTC Alarm A Interrupt 
EXTI_ClearITPendingBit(EXTI_Line17 ); 
EXTI_InitStructure.EXTI_Line = EXTI_Line17; 
EXTI_InitStructure.EXTI_Mode = EXTI_Mode_Interrupt; 
EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger_Rising; 
EXTI_InitStructure.EXTI_LineCmd = ENABLE; 
EXTI_Init(&EXTI_InitStructure); 
/* Enable the RTC Alarm Interrupt */ 
NVIC_InitStructure.NVIC_IRQChannel = RTC_Alarm_IRQn; 
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 4; 
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; 
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; 
NVIC_Init(&NVIC_InitStructure); 
#endif 
return RTC_ConfigState; 
} 
/******************************************************************************* 
* 
* @fn RTC_SetCompilationDate 
* @brief Set compilation date to RTC 
* Author: kawel 
* 06-06-2014 
* @warning none 
* 
* @param void 
* 
* @return void 
* 
*******************************************************************************/ 
void RTC_SetCompilationDate(void) 
{ 
uint8_t day, month, year; 
int WeekDay; 
RTC_DateTypeDef RTC_DateStructure; 
debug_printf(_LVL_3, ''Compilation date: %s \r\n'', __DATE__); 
if (RTC_GetDateFromCompilationDate(&day, &month, &year) == SUCCESS) 
{ 
RTC_DateStructure.RTC_Date=day; 
RTC_DateStructure.RTC_Month=month; 
RTC_DateStructure.RTC_Year=year; 
WeekDay=RTC_CalcDayOfWeek2(&RTC_DateStructure); 
RTC_DateStructure.RTC_WeekDay=WeekDay; 
RTC_SetDate(RTC_Format_BIN, &RTC_DateStructure); 
} 
} 

#stm32f207ve-rtc-date-problem
This topic has been closed for replies.