STM32F207 ETH clock
Hello, I've problem with a clock setting for a MCU. There is some points, which describe it.
General: MCU: STM32F207IGT6
Clock: HSE 8Mhz -> PLL 96Mhz
Using module: ETH MAC - MII 4-bit mode - 25MHz neededFSMC - synchro NOR FLASH mode - 24Mhz must be for a device
Using external device: ETH PHY switch - 88E6060 - own 25Mhz clock – on ETH MAC MII
MVBCS1 - 24Mhz (must be, not configured) on FSMC
Problem: I want to use ETH MAC MII (STM) with ETH PHY switch (88E6060) in MII mode. In this mode, pin TX_CLK and RX_CLK for MII on STM32F207 are as inputs. ETH PHY switch has own clock (external crystal rezonator 25Mhz) and generate clock TX_CLK and RX_CLK for STM32F207. I mean, there is no problem with STM32F207 clock, which is 96Mhz (no divisible 25Mhz). But In this case can be problems with synchronization. In datasheet and reference manual or in forum are not informations for this case. Im not sure with synchro and I need know it without fail
Thanks for a reply