Skip to main content
Nimit Vachhani
Associate III
May 19, 2025 4:08 AM UTC
Solved

STM32F205RG USB High Speed and I2C RTC Problem

Greetings,

In my application i have initialized STM32F205RG with USB High Speed Host for detecting USB Key board and I2C2 for communicating with DS3231 RTC Module. RTC module works prefectly when i don't initialize USB HS peripheral, but when both initialized in the project then I2C2 always sends me HAL_BUSY state.

Is there any solution or work around for this problem ? 

I am using cube mx for code generation and initialiazation. 

Thanks.

 

This topic has been closed for replies.
Nimit Vachhani
Nimit VachhaniBest answer
Associate III
May 20, 2025 5:15 AM UTC

Greetings mbarg.1 ..

Thanks for the advice. Actually i am sorry to bother here on forum as just now i have received new module for DS3231 and it is working fine. May be the rtc module might have been damaged. 

I don't like modules but as i am developing proto type i rely on module to expediate the coding process. Things are now working normal as it should by replacing it with new module.

Thanks again.

6 replies

mbarg.1
Senior III
May 19, 2025 5:00 AM UTC

I do use the same configuration with STM32F7 and with 3 I2c devices (DS3231 + PCA9555D) but I do not see any problem.

Did you check that buffers areas do not overlap or overflow?

HAL_BUSY is device specific - on I2C or USB?

Nimit Vachhani
Associate III
May 19, 2025 6:13 AM UTC

HAL_BUSY  is for I2C... Can please elaborate more on buffer areas...

mbarg.1
Senior III
May 19, 2025 11:06 AM UTC

I2C and USB both save data in buffers - buffers can overflow and corrupt areas with settings - same if overlap