Skip to main content
CLee.5.54
Associate
May 20, 2019
Question

STM32F205 revision V has some weak GPIO port from ESD.

I use STM32F205ZGT6 for our product.  

In our design, PH10 and PH11 is connected external module. When external connected, the port get physical damage in only revision V. I checked that the other revision such as 1 , 2 and 3 don't have same issue.

I set PH10 and PH11 port as alternate function, Open-drain, Pullup and Active Low.

I hope to know this issue is reported or not to STM and what differ between revision V and others.

There are no mention about this issue in errata sheet. 

https://my.st.com/content/my_st_com/en/products/microcontrollers-microprocessors/stm32-32-bit-arm-cortex-mcus/stm32-high-performance-mcus/stm32f2-series/stm32f2x5/stm32f205zg.html#resource

This topic has been closed for replies.

4 replies

Amel NASRI
ST Technical Moderator
May 24, 2019

Hello @CLee.5.54​ ,

As there is no particular issue already known for STM32F205ZGT6 rev V, the problem you are reporting needs to be investigated.

So, could you please

  • share the schematic of your board?
  • provide the trace code of device(s) having the issue? Do all devices with the problem have the same date code?
  • Is the problem seen on all rev V devices, or some of them are working properly?

Thanks,

Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
CLee.5.54
CLee.5.54Author
Associate
May 27, 2019

Hello Amel

​

please find the information in my attachment. I put a part of schematic and internal test information in. 

Under our test that connect external module on 5 times, Defect rate is about 85% ( 13 defect / 15 samples ).

Amel NASRI
ST Technical Moderator
May 27, 2019

Hi Chikang,

The attachment is well received. It will be reviewed by our experts.

Would it be possible to complete the marking of other devices (rev V)?

Thanks,

Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.