Skip to main content
root
Associate III
June 8, 2012
Question

[STM32F205] MCU is doing a lot more work since last firmware, how to I debug ?

  • June 8, 2012
  • 1 reply
  • 497 views
Posted on June 08, 2012 at 11:03

Hello,

I'm having a strange issue ... when I upgrade from firmware X to firmware Y, the MCU is consumming more amps (board consumption from 50mA to 80mA), and generates more heat (from 42°C to 50°C).

I checked a hundred time the differences in code, and cannot see any reason for this. Application is still running fine though ...

Any clue on how to debug this ? I'm using TASKING and I have ST Link V2 probes and SEGGER probes at hand.

Thomas.
    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    June 8, 2012
    Posted on June 08, 2012 at 13:47

    With that much current I'd be looking very carefully at what the GPIO ports were doing. If there were some issues with AF settings, or pins fighting. Or generally what the GPIOs were driving, especially if the current if for the system, rather than just the CPU.

    Presumably you've compared the entire source trees with merge tools like WinMerge or Araxis Merge, etc.

    The other trick might be to build an intermediate firmware where you pull some subset of the changes and see at what point the current usage changes.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..