Skip to main content
Pranay Dhuri
Associate III
June 30, 2018
Question

STM32F2 MCU as I2C master unable to communicate with I2C slave devices with 7 bit I2C address between 120-124

  • June 30, 2018
  • 4 replies
  • 1152 views
Posted on June 30, 2018 at 07:42

Hi,

I have implemented I2C master on STM32F207VG and performing I2C bus scan for slave detection.

I am having a slave device whose I2C address can be modified.

It is working fine with all addresses except addresses 120,121,122,123,124. When I change my slave I2C address to any of these, STM32 fails to detect it, whereas when I am testing same device with Arduino as master it is being detected on bus.

Are there any limitations on I2C slave addresses with STM32 controller?

If no, then what can be reasons for not responding to particular address range.

Thanks in advance.

    This topic has been closed for replies.

    4 replies

    T J
    Senior III
    June 30, 2018
    Posted on June 30, 2018 at 14:52

    only to say ,

    1. make sure you are 100KHz or under to be well within operating speed.

    2. no long wires.nothing over 2cm or else you are the problem. drop your speed again

    3. strong pullups help, try 1K pullup.

    how many devices on the bus ?

    Pranay Dhuri
    Associate III
    July 2, 2018
    Posted on July 02, 2018 at 08:54

    Hi T J, I am operating I2C bus at 100KHz, I have tested with only one device on bus. Problem is arriving, if i modify slave address between 120 -124.

    Tesla DeLorean
    Guru
    July 3, 2018
    Posted on July 03, 2018 at 14:22

    Stick a scope on the pins, and confirm a) the address sent, and b) the response from the slave via ACK

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Danish1
    Lead III
    July 2, 2018
    Posted on July 02, 2018 at 13:43

    Looking at the I2C specification

    https://www.nxp.com/docs/en/user-guide/UM10204.pdf

     section 3.1.11, I think 7-bit addresses 0b11110xx are forbidden because they are used to indicate a 10-bit address being used.

    Can the Arduino cope with 10-bit I2C addresses? If not it might wrongly allow that sequence as a 7-bit address. But stm32 should properly handle 10-bit addresses.

    Hope this helps,

    Danish