Skip to main content
Gabriel Germanovix
Associate II
February 23, 2014
Question

STM32F1xx - How to implement moving average - SOLVED

  • February 23, 2014
  • 5 replies
  • 3122 views
Posted on February 23, 2014 at 16:42

The original post was too long to process during our migration. Please click on the attachment to read the original post.
    This topic has been closed for replies.

    5 replies

    francescatodiego
    Associate III
    February 23, 2014
    Posted on February 23, 2014 at 18:47

    What does not work?

    http://en.wikipedia.org/wiki/Moving_average

    We describe some possible formulas

    I used the moving average window

    You need to store N consecutive samples where N is the width of the window

    The average value is

    Mn +1 = Mn - sample (n - N) / N + sample (n +1) / N

    or in the best form

    N * Mn +1 = N*Mn - sample (n - N) + sample (n +1)

    and divide by N only when necessary. (

    But you must be careful N*Mn must be stored in 32bit ma

    x)

    In other words, remove from the average the buffer oldest value and add the last measure

    Sample data buffer can be implemented with a circular buffer.

    ( last measure replaces the oldest value and you can easily calculate the above formula )

    At powerup

    fill ALL the data buffer with 

    the first A/D measure (This prevent the startup delay caused by average )

    If possible, for evrey measure exec multiple high speed A/D conversions and

    performs the average of these measures

    Normally  I exec 10 high speed A/D conversion I subtract the min and the max values ​​and I shift right 3 time (8 divide) the results

    This value is my new sample.

    ks..
    Gabriel Germanovix
    Associate II
    February 24, 2014
    Posted on February 24, 2014 at 01:42

    Thanks for explanations... and wiki link.. but not solved the problem

    Gabriel Germanovix
    Associate II
    February 27, 2014
    Posted on February 27, 2014 at 02:17

    Hello Diego,

    In terms of functions, interrupts and config things.. Did you have any example to show?

    In my codes i divide the buffer on two parts:

    The newest and the oldest part...

    When the interruptions (HT or TC) are called the other half of buffer is subtracted and current part is added. (see the interruption of DMA)

    I stored a certain amount of data and then do the calculations .. 

    The initial values ​​are correct but after some time the values ​​begin to show errors. If the input voltage varies widely the error is even greater. 

    Even though I keep constant signal after a large variation results are never consistent. Only resetting the module restore the correct values of average.

    Tkz...

    francescatodiego
    Associate III
    February 27, 2014
    Posted on February 27, 2014 at 09:05

    germanovix

    for me it is impossible to find a problem just by reading some of the code without debugging support

    I would do this:

    Control the number and sequence of the DMA interrupt eg using counters that increments on flags HT and CT ( If you lose a few interrupts as you see it )

    Control of the data buffer .

    I would use only two input values ​​(eg two batteries 1.2V and 2.4V ) each time you fill a buffer check that all the values are correct .

    Start acquisitions test at very low frequency to verify interrupt dma etc.

    If you have free ram created a temporary buffer where download all

    acquired

    data, or if possible send buffer to serial port

    I do not know if there is an error in the calculations but to do a test: create a know data buffer (ex a ramp) calculate the moving average for te know buffer and save all the results in another buffer

    Remove the DMA transfer and work with conversion complete interrupt

    Another test

    add increment counter in DMA interrupt and

    decrement counter when data is processed

    When you start buffer processing the counter value must be 1 (not > 1)

    frankmeyer9
    Associate III
    February 28, 2014
    Posted on February 28, 2014 at 10:17

    The initial values ​​are correct but after some time the values ​​begin to show errors. If the input voltage varies widely the error is even greater. 

     

     

    Even though I keep constant signal after a large variation results are never consistent. Only resetting the module restore the correct values of average.

    Sounds to me like an overflow in your calculation.

    However, I suggest to separate your issues. Pull your moving-average implementation/functions out and test them on a PC. I'm using the CodeBlocks IDE for such purposes. This lets you feed the algorithm with simulated input data, watch the intermediate results in the debugger, and verify it.

    Only then I would go on to check if the input data feed (ADC/DMA) is correct.