Skip to main content
denlok
Associate II
March 13, 2012
Question

STM32F1xx and STM32F2xx HSI stability

  • March 13, 2012
  • 3 replies
  • 850 views
Posted on March 13, 2012 at 16:47

Hello! I have a question to STM32xx chip manufacturers.

Last yar I uses STM32F10xx chips in my applications. It's 8mHz HSI works perfect - stable, with small temperature sensistivity - works very well.  CAN bus (slow) works perfect on these chips without crystals!

Now I decide to change chips to modern 32F2xxx, but after testing I see it's HSI works pure - very temperature/voltage sensitive, and somthing else...

In my application:

VCAP1 = 2.2uF

VCAP2 = 2.2uF

VDD1...5, VREF+ connects to 3.3v with 100uF capacitor

I have written the chip temp. monitoring loop in my application programm, but it helps to stabilize HSI frequency only for 60% chips (by manufacturer tape pack). 40% chips can't work anywhere..

Can someone say any way to make HSI stable same as STM32F10xx serie?

#stm32f2-hsi-problems
    This topic has been closed for replies.

    3 replies

    emalund
    Associate III
    March 13, 2012
    Posted on March 13, 2012 at 19:22

    (CAN) bus, demands communication accuracy of less than ±1.0 percent because the microcomputers used are equipped with this high-speed communication function. Specifically, when a CAN-bus performs high-speed communications of 500Kbps, an accuracy of ±0.3 percent or less is required for a resonator used in the ECU.

     

    The datasheet for the f1xx do not guarantee it to work within these limites.that it happened to was a matter of luck.

    ''design by test'' is guaranteed to bite you where you sit eventually.

    THUS, if the f2xx stay within the limits stated in the datasheet, you have no course of action.

    Erik

    Tesla DeLorean
    Guru
    March 13, 2012
    Posted on March 13, 2012 at 22:51

    The STM32F1's HSI was specified as 1% typical, the STM32F4 is specified as 1%. It's trimmed, but at some arbitrary temperature, and is not temperature compensated.

    The LSI on the F1's is 40 KHz, (30 - 60 KHz) @ 20-50%

    None of these are adequate for CAN if you expect 0.3% , especially across industrial/car temperature profiles. What's the problem with using a crystal or TCXO?

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    denlok
    denlokAuthor
    Associate II
    August 5, 2012
    Posted on August 05, 2012 at 08:55

    My task was a make data converter with dimensions smaller as possible.

    Problem was solved, the reason of HSI big drift was simple - as minimum one Low-Freqency capacitor bigger than 5uF must be mounted near microcontroller 3.3V power pins.