Skip to main content
tdropka
Associate
January 24, 2014
Question

STM32F10xxx firmware library V2.0.1

  • January 24, 2014
  • 2 replies
  • 987 views
Posted on January 24, 2014 at 18:46

Is the STM32F10xxx firmware library (FWLib) version 2.0.1 available anywhere? The ''STM32 Legacy Firmware Libraries'' page starts at 2.0.3, but I need to port an application from 2.0.1 to StdPeriph_Lib v3.5.0 and I need to see what modifications the original developer made to 2.0.1. There were enough changes between 2.0.1 and 2.0.3 that I can't tell which ones were his.

Thanks, Tom
    This topic has been closed for replies.

    2 replies

    Tesla DeLorean
    Guru
    January 24, 2014
    Posted on January 24, 2014 at 20:37

    These are the V2.0.1 files I have repackaged

    ________________

    Attachments :

    STM32F10xFWLib_V2.0.1.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0qs&d=%2Fa%2F0X0000000beS%2Fsf1HAAJURsKE5hzjN_LRYwszkKQhHdkKSCa1pX579hk&asPdf=false
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    tdropka
    tdropkaAuthor
    Associate
    January 24, 2014
    Posted on January 24, 2014 at 20:45

    Thank you very much, clive1. That was exactly what I needed.

    Tom