Skip to main content
stst9187
Associate III
Jan 4, 2013 5:18 PM UTC
Question

STM32F10x_StdPeriph_Lib_V3.5.0 & IAR v6.5

Posted on January 04, 2013 at 18:18

Hi

I'm using STM32F10x_StdPeriph_Lib_V3.5.0 with IAR 6.50 compiler but when I open the workspace in the templade directory and then I build it ,  I found 240 errors look like these :

Building configuration: Project - STM3210C-EVAL 

Updating build tree... 

main.c  

Error[Pe147]: declaration is incompatible with ''__nounwind __interwork __softfp unsigned long __get_PSP(void)'' (declared at line 52 of ''C:\Program Files\IAR Systems\Embedded Workbench  C:\progetti\file-rete\STM32F10x_StdPeriph_Lib_V3.5.0\Libraries\CMSIS\CM3\CoreSupport\core_cm3.h 1084 

6.5\arm\inc\c\intrinsics.h'') 

Error[Pe147]: declaration is incompatible with ''__nounwind __interwork __softfp void __set_PSP(unsigned long)'' (declared at line 53 of ''C:\Program Files\IAR Systems\Embedded Workbench  C:\progetti\file-rete\STM32F10x_StdPeriph_Lib_V3.5.0\Libraries\CMSIS\CM3\CoreSupport\core_cm3.h 1094 

6.5\arm\inc\c\intrinsics.h'') 

Can You help me?

thanks
    This topic has been closed for replies.

    2 replies

    Tesla DeLorean
    Guru
    Jan 4, 2013 6:34 PM UTC
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    stst9187
    stst9187Author
    Associate III
    Jan 6, 2013 9:44 PM UTC
    Posted on January 06, 2013 at 22:44

    thanks very much!