Skip to main content
redkofka
Associate II
June 18, 2012
Question

stm32f10x DMA RX Interupt ....

  • June 18, 2012
  • 2 replies
  • 762 views
Posted on June 18, 2012 at 07:40

HI I want to use DMA to Recieving data via uart (rs485)

 I want to use 20byte buffer but for siplicity in this exaple is shown only 1byte buffer...

 int main(void){

 RCC_Configuration();

 GPIO_Configuration();

 USART_Configuration();

 DMA_Configuration();

 NVIC_Configuration_DMA_RX();

 while(1){

 };

 }

 /******************************************************************************/

 void RCC_Configuration(void)

 {

 /* Enable DMA clock */

 RCC_AHBPeriphClockCmd(RCC_AHBPeriph_DMA1, ENABLE);

 /* Enable GPIO bank clock */

 RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE);

 /* Enable UART clock */

 RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1, ENABLE);

 }

 /******************************************************************************/

 void GPIO_Configuration(void)

 {

 GPIO_InitTypeDef GPIO_InitStructure;

 /* Configure USART Tx as alternate function push-pull */

 GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9; // PA.09 USART1.TX

 GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP;

 GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

 GPIO_Init(GPIOA, &GPIO_InitStructure);

 /* Configure USART Rx as input floating */

 GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10; // PA.10 USART1.RX

 GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING;

 GPIO_Init(GPIOA, &GPIO_InitStructure);

 }

 /******************************************************************************/

 void USART_Configuration(void)

 {

 USART_InitTypeDef USART_InitStructure;

 /* USART resources configuration (Clock, GPIO pins and USART registers) ----*/

 /* USART configured as follow:

 - BaudRate = 115200 baud

 - Word Length = 8 Bits

 - One Stop Bit

 - No parity

 - Hardware flow control disabled (RTS and CTS signals)

 - Receive and transmit enabled

 */

 USART_InitStructure.USART_BaudRate = 115200;

 USART_InitStructure.USART_WordLength = USART_WordLength_8b;

 USART_InitStructure.USART_StopBits = USART_StopBits_1;

 USART_InitStructure.USART_Parity = USART_Parity_No;

 USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_RTS;

 USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;

 /* USART configuration */

 USART_Init(USART1, &USART_InitStructure);

 /* Enable the USART1 */

 USART_Cmd(USART1, ENABLE);

 USART_ITConfig(USART1, USART_IT_RXNE, ENABLE);

 /* Enable DMA Requests*/

 USART_DMACmd(USART1, USART_DMAReq_Rx, ENABLE);

 USART_DMACmd(USART1, USART_DMAReq_Tx, ENABLE);

 }

 /******************************************************************************/

 /**

 * @Brief

 * @Parameter None

 *

 * @Return None

 */

 void DMA_Configuration(void)

 {

 // USART1 Channel 4, USART2 Channel 7, USART3 Channel 2

 /***TX********************/

 DMA_DeInit(DMA1_Channel4);

 DMA_Cmd(DMA1_Channel4, DISABLE);

 /***RX********************/

 DMA_DeInit(DMA1_Channel5);

 DMA_Cmd(DMA1_Channel5, DISABLE);

 }

 /******************************************************************************/

 void DMA_USART_Rx (void){

 DMA_InitTypeDef DMA_InitStructure;

 DMA_DeInit(DMA1_Channel5);

 DMA_InitStructure.DMA_PeripheralBaseAddr = (u32)&USART1->DR;

 DMA_InitStructure.DMA_MemoryBaseAddr = (u32)RXpacket;

 DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralSRC;

 DMA_InitStructure.DMA_BufferSize = 1; //20 in the end

 DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;

 DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;

 DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Byte;

 DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_Byte;

 DMA_InitStructure.DMA_Mode = DMA_Mode_Normal;

 DMA_InitStructure.DMA_Priority = DMA_Priority_High;

 DMA_ITConfig(DMA1_Channel5,DMA_IT_TC,ENABLE);

 DMA_InitStructure.DMA_M2M = DMA_M2M_Disable;

 DMA_ClearFlag(DMA1_FLAG_TC5);

 DMA_Init(DMA1_Channel5, &DMA_InitStructure);

 DMA_Cmd(DMA1_Channel5, ENABLE);

 /* Wait of DMA completion */

 USART_Cmd(USART2, ENABLE);

 DMA_ITConfig(DMA1_Channel5, DMA_IT_TC , ENABLE);

 while(DMA_GetFlagStatus(DMA1_FLAG_TC5) == RESET);

 /* Loop until the end of transmit */

 while(USART_GetFlagStatus(USART1, USART_FLAG_TC) == RESET);

 }

 /******************************************************************************/

 void NVIC_Configuration_DMA_RX(void)

 {

 NVIC_InitTypeDef NVIC_InitStructure;

 //Enable the USARRx Interrupt

 NVIC_InitStructure.NVIC_IRQChannel = DMA1_Channel5_IRQn ;

 NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 1;

 NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1;

 NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;//ENABLE

 NVIC_Init(&NVIC_InitStructure);

 /******************************************************************************/

 void DMA1_Channel5_IRQHandler(void)

 {

 /*This part never start*/

 }

 /******************************************************************************/

 BUT WHEN I USED :

 /******************************************************************************/

 void NVIC_Configuration_Irq(void)

 {

 NVIC_InitTypeDef NVIC_InitStructure;

 //Enable the USART_Rx Interrupt

 NVIC_InitStructure.NVIC_IRQChannel = USART1_IRQn;

 NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;

 NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;

 NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;//ENABLE

 NVIC_Init(&NVIC_InitStructure);

 }

 /******************************************************************************/

 void USART1_IRQHandler(void) //Reading data

 {

 GPIO_WriteBit(LED_PORT, GPIO_Pin_13, Bit_SET);

 if ((USART1->SR & USART_FLAG_RXNE) != (u16)RESET);

 DMA_USART_Rx();

 }

 /******************************************************************************/

  iTS FIRST TIME GO IN USART1 INTERUPT AND THEN IN DMA1_Channel5....

  sorry about your time but i cant find some DMA Rx example .....

 second problem is that i want to use 20byte buffer - but in debugger always i recieve only firt

 i use -DMA_InitStructure.DMA_BufferSize = 20; and in debugger i see that first is recieved bud only firt

 isnt problem that dma cant read whole buffer -its read one by one ?

 somewhere i read that the DMA_IT_TC is possible to use only in M2M mode ....

 would you be so kind and take a look at code

 thanks
    This topic has been closed for replies.

    2 replies

    alok472
    Associate
    June 18, 2012
    Posted on June 18, 2012 at 15:38

    Suggest to download STM32F2xx Standard Peripheral Library example ?For USART, there is an example of 2 boards communication.

    (\USART\USART_TwoBoards\DataExchangeDMA)

    The readme.txt says ''In both boards, the data transfers is managed using the USART Tx/Rx channels DMA requests.''

    hope it helps

    redkofka
    redkofkaAuthor
    Associate II
    June 26, 2012
    Posted on June 26, 2012 at 08:50

    thanks i ll check it.