X axis : 13=-2, 14=-1, 15=right ADC value, 16=+1 17+2 and so on
Y axix : number of hits you see I wrote: here are the ADC result displayed as accumulated hits in distance from right value, but ok the 15 = centre value was not really explained, sorry. both plots taken over the same time unit, see the number of correct hits are 60 and 275 quite a big difference.
if you use the cool board : STM32F10F10X-128K-EVAL
and if you like to experiment with ADC you should disconnect the LCD. here are the ADC result displayed as accumulated hits in distance from right value, with LCD and without.
no LCD on ST kit I have also tested other dev boards like the keil board and the circle, both also add noise to the ADC, due to switched power supply or long tracks to critical analog CDD and analog GND. so keep this in mind if you need full ADC resolution. Yours: Thomas Scherrer - OZ2CPU Denmark - www.webx.dk [ This message was edited by: tta on 13-02-2008 15:53 ] [ This message was edited by: tta on 13-02-2008 16:01 ]
this is the onboard potentiometer connected to ADC14 on the eval board. and when the LCD is connected in the socket, NOT initialized or anything, ONLY power applied, all IO pins are non switching during this test ! PS: how did you put that picture on your profile ? I cant find it ?[ This message was edited by: tta on 14-02-2008 17:19 ]
thanks :) >did you try to run the A/D using DMA with the Core disabled? >That would be an interesting test. ?? why would that be interesting ? the test show 100% of the noise is comming from the LCD switcher ! when I remove the LCD I have under 1LSB of noise at 12bits, that is with DMA and ADC and CPU running at full speed ! it is impossible to have zero bits of jitter, at any input voltage, you see if you simply set the ADC voltage to a voltage centre aligned to ½LSB that bit will flip all the time with ½ your sample rate, and same issue witl 1/3 of and LSB and so on :)
On 14-02-2008 at 08:35, Anonymous wrote: X axis : 13=-2, 14=-1, 15=right ADC value, 16=+1 17+2 and so on Y axix : number of hits you see I wrote: here are the ADC result displayed as accumulated hits in distance from right value, but ok the 15 = centre value was not really explained, sorry. both plots taken over the same time unit, see the number of correct hits are 60 and 275 quite a big difference. Ok, that's some good data, did you try to run the A/D using DMA with the Core disabled? That would be an interesting test. I have used some Analog Devices micros with 12 bit A/D's and could get it so no bits would flip on LSB bit with the core running, but those chips were basically high quality A/D's with a core wrapped around it as an after thought, they sacrificed everything to make that A/D perform. Silabs are similar, I believe, but never used them. It's very hard to make a good A/D on the same chip as a CPU, there are conflicting requirements (die material that is good for an A/D is bad for a CPU)
I am sorry but the profile has been created long time ago and I don't remember how it has been done.
I think this noise is related to the step-up regulator used to supply the backlight LEDs. This ADC input line is very long on the board since the corresponding IO is connected to the daughter board connector and to potentiometer far from the MCU. Such general purpose board is not designed for analog signals optimization. Maybe a simple low pass filter close to the MCU should improve the noise immunity but in this case the corresponding IO is no more usable as digital signal. Regards,
it dont have the bargraph mode yet, it draws connected lines from points, but I will add it to the idea list. [ This message was edited by: tta on 18-02-2008 19:28 ]
On 18-02-2008 at 09:17, Anonymous wrote: >Ok, that's some good data, thanks :) >did you try to run the A/D using DMA with the Core disabled? >That would be an interesting test. ?? why would that be interesting ? the test show 100% of the noise is comming from the LCD switcher ! when I remove the LCD I have under 1LSB of noise at 12bits, ok, I thought the graph showed you have a spread of 5 counts, but looking at it again that is not true, my mistake (probably would of been better as a bar chart)