Skip to main content
rybaryba
Associate
September 4, 2015
Question

STM32F107VCT6 - programming via USART1

  • September 4, 2015
  • 4 replies
  • 945 views
Posted on September 04, 2015 at 18:20

Dears,

I've got Core107V board from Waveshare with STM32F107VCT6 (rev.Z) and I want to flash my program using USART1.

I've plugged FTDI converter the board according to the information in datasheet.

3.3V => 3.3V on Core107V

GND => GND on Core107V

TX => PA10

RX => PA9

BOOT0 and BOOT1 are set correctly for sure.

I've used standard setting in ST Downloader Demo, Baud: 115200, Parity Even, timing 5, data bits 8.

Unfortunately ST Downloader says it cannot connect to the board (No response from target).

Could u pls give me any advice how to get it connected?

Please see the board:

http://www.wvshare.com/img/devkit/Core107V/Core107V-intro-1.jpg

Regards,

Tomek

    This topic has been closed for replies.

    4 replies

    Tesla DeLorean
    Guru
    September 4, 2015
    Posted on September 04, 2015 at 18:35

    Check the supply voltages.

    Make sure you reset the board immediately before you try to connect, and each time you retry.

    Consider using something like RealTerm, and in Hex mode send an 0x7F byte, and observe the response from the board.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    rybaryba
    rybarybaAuthor
    Associate
    September 4, 2015
    Posted on September 04, 2015 at 19:24

    Hi,

    uC power is supplied from FTDI converter (USB). Is it ok?

    And I checked with real term. Nothing got after sending 0x7F (hex, send number).

    But after reset I got ''00''

    Regards,

    Tomek

    Tesla DeLorean
    Guru
    September 4, 2015
    Posted on September 04, 2015 at 19:30

    Then you're down to mundane things like double checking exactly what state BOOT0/BOOT1 are at the device pins.

    And scoping some of the signals. Confirm it's being powered as you expect.

    Make sure the FTDI doesn't have the RX/TX sense reversed, confirm what way the data from the PC comes, send a continuous stream of U characters, review the signal on a scope.

    Review a board schematic, try programming with JTAG/SWD

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    rybaryba
    rybarybaAuthor
    Associate
    September 6, 2015
    Posted on September 06, 2015 at 16:23

    Hi Clive,

    Thanks for your effort and advices.

    The problem has been solved. It seems it was HW problem, which is decribed in the document AN2606.

    My chip version 344 has some problems with running bootloader. Version above 937 doesn't have it.

    The solution is as follows:

    - If using USART2 for communicating, put +3.3V on: PA10, PA11, PA12 and PD6.

    Anyway thanks to you I learned RealTerm which seems to be very usefull tool now for me! :)

    Regards,

    Tomek