Skip to main content
hakeila9
Visitor II
December 7, 2012
Question

STM32F107VC USART Transmit register

  • December 7, 2012
  • 1 reply
  • 496 views
Posted on December 07, 2012 at 06:46

Hi,

I am trying to communicate to STM32F107VC microcontroller via UART5. I am debugging the DR register of UART5 port, but it seems it is always zero (I am using IAR EWARM with ST-LINK V2 via STM32F1Discovery).

the PCLK1 is configured to be 31.25 MHz

Here is my code:

main.c:

--------

/* Setup STM32 system (clock, PLL and Flash configuration) */

  RCC_init();

  IO_init();

  USART_init();

  //EXT_CRT_SECTION();

  // send test data to USART1

 

/* Infinite loop */

  while (1)

  {    

    // send test data via USART1

    USART_SendData(UART5, (uint16_t)'T');

    while(USART_GetFlagStatus(UART5,USART_FLAG_TXE) == RESET); // wait until the TDR (Tx register) data is transfered to the shift register

        

    LED_Test();

    

     } 

}

--------------------------------------------------------------------------------------------

init.c:

-----

void USART_init(void)

{

  GPIO_InitTypeDef GPIO_InitStructure;

  USART_InitTypeDef USART1_InitStructure;

  USART_InitTypeDef UART5_InitStructure;

 

  // Release reset and enable clock

  USART_DeInit(UART5);

  RCC_APB1PeriphClockCmd(RCC_APB1Periph_UART5, ENABLE);

 

  RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOD,ENABLE);

  RCC_APB2PeriphResetCmd(RCC_APB2Periph_GPIOD,DISABLE);

 

  RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOC,ENABLE);

  RCC_APB2PeriphResetCmd(RCC_APB2Periph_GPIOC,DISABLE);

 

 

  /* UART5 Configuration

   *=====================*/

  // configure the IO ports for UART5 Tx as output

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_12;

  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP;

  GPIO_Init(GPIOC, &GPIO_InitStructure);

 

  // configure the IO ports for UART5 Rx as input

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2;

  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING;

  GPIO_Init(GPIOD, &GPIO_InitStructure);

 

  // configure the UART5 serial registers

  UART5_InitStructure.USART_BaudRate = 115200;

  UART5_InitStructure.USART_WordLength = USART_WordLength_8b;

  UART5_InitStructure.USART_StopBits = USART_StopBits_1;

  UART5_InitStructure.USART_Parity = USART_Parity_No;

  UART5_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;

  UART5_InitStructure.USART_Mode = USART_Mode_Tx | USART_Mode_Rx;

  USART_Init(UART5,&UART5_InitStructure);

 

 

  // enable UART5

  USART_Cmd(UART5, ENABLE);

} stm32f10x_usart.c

------------------

void USART_SendData(USART_TypeDef* USARTx, uint16_t Data)

{

  /* Check the parameters */

  assert_param(IS_USART_ALL_PERIPH(USARTx));

  assert_param(IS_USART_DATA(Data));

   

  /* Transmit Data */

  USARTx->DR = (Data & (uint16_t)0x01FF);

}

    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    December 7, 2012
    Posted on December 07, 2012 at 13:44

    So, DR means different things depending if your reading or writing. When reading your are seeing the RECEIVED data, which would come from the PC or other external source.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..