Question
STM32F107 Virtual Com example - echo needed
Posted on December 27, 2012 at 09:59
Hi!
I have a problem with usage of ST-example for Virtual Com port. I have STM32F107 on my board. Example is downloaded correctly and all seems workable. The thing is that my board is not standard evaluation board and it doesn't use USART. So, I decided to change example code to make it work without USART - only with USB. I'd lile to make Echo-program: device should return back all bytes, received from PC. In the code I see sevearl places, where data is sended or received from USB: 1. EP1_IN_Callback (void) 2. EP3_OUT_Callback(void) 3. Handle_USBAsynchXfer (void) Two moments need clarification: 1. in EP3_OUT_Callback(void) i retranslate data, received from USB on EP3 to USB on EP1 instead of USART. Is it correct way?...
USB_Rx_Cnt = USB_SIL_Read(EP3_OUT, USB_Rx_Buffer); USB_SIL_Write(EP1_IN, USB_Rx_Buffer, USB_Rx_Cnt); SetEPTxValid(ENDP1); ... 2. The problem I encounter here, is that program crashes any time after usage of USB_SIL_Write, cycling in the HardFault_Handler function. What can be reason of it? It would be great if anyone gives me any advices concerning this points. Thanks in advance!