STM32F107 can't correctly wakeup from standby mode
I'm trying to use the standby mode of STM32F and waking it up by WKUP (PA0) pin.
Going to standby seems OK, power consumption goes to 4 uA.
If I reset MCU with RESET pin, it starts normally: after 250 ms delay it goes to sleep and consumes 4 uA
https://i.stack.imgur.com/nDM6f.png
But if I wake it up with WKUP pin it behaves strangely: consumption stays on a "run" level and I see cycles off my 250 delay, MCU keeps restarting instead of going to sleep.
https://i.stack.imgur.com/KYPqM.png
My code is really simple:
#include <stm32f1xx_hal.h>
#ifdef __cplusplus
extern "C"
#endif
void SysTick_Handler(void)
{
HAL_IncTick();
HAL_SYSTICK_IRQHandler();
}
void Error_Handler()
{
__asm("bkpt 255");
__asm("bx lr");
}
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = { 0 };
RCC_ClkInitTypeDef RCC_ClkInitStruct = { 0 };
__HAL_RCC_AFIO_CLK_ENABLE();
__HAL_RCC_PWR_CLK_ENABLE();
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI | RCC_OSCILLATORTYPE_LSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.LSIState = RCC_LSI_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
RCC_OscInitStruct.PLL2.PLL2State = RCC_PLL_NONE;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_SYSCLK
| RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
{
Error_Handler();
}
/** Configure the Systick interrupt time
*/
__HAL_RCC_PLLI2S_ENABLE();
}
int main(void)
{
HAL_Init();
SystemClock_Config();
__HAL_AFIO_REMAP_SWJ_NOJTAG();
HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN1);
HAL_Delay(250);
HAL_PWR_EnterSTANDBYMode();
}