Skip to main content
ron
Visitor II
March 14, 2014
Question

STM32F107 as a USB Virtual COM Port Device

  • March 14, 2014
  • 1 reply
  • 583 views
Posted on March 14, 2014 at 21:29

If I set up the STM32F107 as a USB Virtual COM Port Device (using for instance ''stm32_f105-07_f2_f4_usb-host-device_lib.zip''), do I need to install the Virtual COM Port driver for it to function with Windows 7?

UM1021 which describes the above firmware package indicates that the VCP driver is required, but I'm wondering if that was based on perhaps WinXP, and maybe the driver is built-in to Win7?

Any comments would be most appreciated.

    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    March 14, 2014
    Posted on March 14, 2014 at 21:49

    No, I'm pretty sure you're going to have to install the appropriate 32-bit or 64-bit driver for Win7

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..