Skip to main content
Treacy Yao
Associate III
Jul 9, 2018 7:45 AM UTC
Solved

stm32F105RB flash range

Posted on July 09, 2018 at 09:45

Hello,

I have stm32F105RB with 128KB flash and 64KB sram. But I qury the related document, the flash organization is as below which total flash size is 256KB. Are there any other documents to introduce the 128KB flash of 

stm32F105RB

? My undestanding of  

stm32F105RB with 128KB flash

address is 0x08000000-?0x0801FFFF,0x08020000-0x01FFFAFFF is reserved. Am I right?

#stm32f105rb-flash
This topic has been closed for replies.
AvaTar
AvaTarBest answer
Senior III
Jul 10, 2018 8:26 AM UTC
Posted on July 10, 2018 at 08:26

I'm confused. so you mean the STM32F105RBT6(128KB flash, 64KB sram) might have more flash but it can just use 128KB?

This issue had been discussed here some times. It is a matter of economy for ST to sell MCUs as 128kB variants wich have a defect in the second 128kB section. For your question, better ignore that.

 I can't find the related map of 'only to 128KB flash in memory map'.

There is none. Just the mentioned datasheet and reference manual for the F105/F107 parts, which describe the address map for the maximal variant.

MCU variants with less Flash just use only the lower parts/sectors (addresses), and the rest is reserved.

Remember, this series is about 10 years old.

8 replies

AvaTar
Senior III
Jul 9, 2018 8:41 AM UTC
Posted on July 09, 2018 at 10:41

But I qury the related document, the flash organization is as below which total flash size is 256K.

Not sure what you mean.

Check the datasheet, downloadable here :

https://www.st.com/en/microcontrollers/stm32f105rb.html

 

Page 33 has a mamory map, with Flash from 08000000 - 0803FFFF.

Treacy Yao
Associate III
Jul 9, 2018 12:24 PM UTC
Posted on July 09, 2018 at 12:24

Yes, 

Page 33 has a mamory map, with Flash from 08000000 - 0803FFFF.

But my STM32F105RB flash is 128KB, not 256KB. so I want to know this one's flash range.
AvaTar
Senior III
Jul 9, 2018 1:39 PM UTC
Posted on July 09, 2018 at 13:39

See the reference manual, sect. 3.3.3.

ST's designation scheme (connectivity,low/medium/high density) for the F1 devices is a bit confusing, and had been dropped for later series.

The device might have more Flash physically, which failed product test.

Tilen MAJERLE
ST Employee
Jul 10, 2018 6:19 AM UTC
Posted on July 10, 2018 at 08:19

Memory map is general for F105 MCU series. As you only have 128kB of flash, take into account only first 128kB of flash in memory map which is in datasheet. Flash starts at address 0x08000000 and is 128kB in size for your MCU.