Skip to main content
duybienle
Associate II
Feb 6, 2017 8:07 AM UTC
Solved

STM32F104RE: how to isntall/use an external clock for the board ?

Posted on February 06, 2017 at 09:07

Hi

I'm using the STM32F401RE Nucleo board, I have noticed that the internal clock HSI has a quite high inaccuracy over temperature and it's not suitable for my application.

I want to use an external clock for the board but I don't know how to properly install and configure the external clock?

And in STM32Cubemx, when selecting SMT32F401RE Nucleo board, in 'Clock Configuration' tab, it's not possible for choosing the HSE clock, only HSI clock available.

Any example on how to use external clock source would be great for me.

Thanks

#external-clock #stm32f401-nucleo #stm32f4 #stm32
This topic has been closed for replies.
Nesrine M_O
Nesrine M_OBest answer
Associate
Feb 6, 2017 9:07 AM UTC
Posted on February 06, 2017 at 10:07

Hi

le.bien

,

STM32Cubemx, when selecting SMT32F401RE Nucleo board, in ''

Clock Configuration

'' tab, it's not possible for choosing the HSE clock, only HSI clock available.

You have first to enable RCC in Pinout tab :

0690X00000606CNQAY.png

Please refer to OSC clock paragraph on

http://www.st.com/content/ccc/resource/technical/document/user_manual/98/2e/fa/4b/e0/82/43/b7/DM001058pdf/files/DM001058pdf/jcr:content/translations/en.DM001058pdf

for more details about the way to configure the pins corresponding to external high-speed clock (HSE) on Nucleo board.

-Nesrine-

Ifmy suggestanswers your question, please mark it as correct.

5 replies

Nesrine M_O
Nesrine M_OBest answer
Associate
Feb 6, 2017 9:07 AM UTC
Posted on February 06, 2017 at 10:07

Hi

le.bien

,

STM32Cubemx, when selecting SMT32F401RE Nucleo board, in ''

Clock Configuration

'' tab, it's not possible for choosing the HSE clock, only HSI clock available.

You have first to enable RCC in Pinout tab :

0690X00000606CNQAY.png

Please refer to OSC clock paragraph on

http://www.st.com/content/ccc/resource/technical/document/user_manual/98/2e/fa/4b/e0/82/43/b7/DM001058pdf/files/DM001058pdf/jcr:content/translations/en.DM001058pdf

for more details about the way to configure the pins corresponding to external high-speed clock (HSE) on Nucleo board.

-Nesrine-

Ifmy suggestanswers your question, please mark it as correct.

Tesla DeLorean
Guru
Feb 6, 2017 12:12 PM UTC
Posted on February 06, 2017 at 13:12

Doesn't the Nucleo have 8 MHz present on the pin from the ST-LINK? Should select HSE BYPASS mode. 

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
duybienle
duybienleAuthor
Associate II
Feb 6, 2017 2:37 PM UTC
Posted on February 06, 2017 at 15:37

Turvey.Clive.002

‌

Yes, I found it in the 64bit Nucleo documentation. However another problem is that after mulitplying in PLL, there is a difference between the theoretical PLLCLK and the actual PLLCLK. Namely:

PLL-setup: /M=8, *N=336, /P=4

- theoretical value PLLCLK = 84MHz

- measured value PLLCLK = 963MHz (using timer interrupt and toggle GPIO pin and measured in Oscilloscope).

Is this a known problem or I missed some specific configuration in the software ?

Thanks

Tesla DeLorean
Guru
Feb 6, 2017 5:10 PM UTC
Posted on February 06, 2017 at 17:10

>>

Is this a known problem or I missed some specific configuration in the software ?

You've missed something, but it is very hard to see from here.

If you want to measure the internal clocks, from the PLL etc, export them via the MCO (PA8) pin and scope them.

The TIM have a toggle mode, this would be a lot less likely to saturate than an interrupt based method. Also be aware Prescaler and Period are N-1 values.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
duybienle
duybienleAuthor
Associate II
Feb 7, 2017 8:40 AM UTC
Posted on February 07, 2017 at 08:40

Yes, my problem was the prescaler value. As you said, it should have used N-1 instead of N.

Thanks